现在电路中只要+5V,想用两款输出-5V电荷泵串连实现-10V的输出,这样是否可行呢!谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
可以的,例如TPS60400系列, 可以看datasheet 第18页figure9-8.
只是反向做,5V输入输出-5V是有偏差的,到-10V偏差可能更大,特别是负载电流较大的情况。
建议你直接用一个降压芯片来做,虽然有额外的电感,可以选择一个较为简单pin脚较少的芯片来做,例如LMR54406,TPS560430之类,将输出接GND, GND就是负压输出。可以参照www.ti.com.cn/.../slva257a.pdf.