Other Parts Discussed in Thread: OPA462
DAC输出±10V 的模拟电压,后级放大到±200V.请问是否有推荐的运放型号?或者参考电路?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,放大输出到+-200V的话,那么运放的供电电压至少也得在+-200V的高压和宽范围,没有这样的运放器件呢。
给您带来不便非常抱歉,或者咨询下“电源管理”版块的电源工程师,是否有参考的boost电路。
单纯看+-150V的输出,可以考虑功放OPA462,宽电压供电范围,最大能达到+-180V,所以+-150V的输出是可以得到的。
同时也要考虑增益带宽积以及压摆率的影响,OPA462的GBW为6.6MHz,如果放大20倍,那么输入信号的频率要小于330Khz,并且还要看下压摆率的影响。
您参考下OPA462的数据手册:https://www.ti.com.cn/lit/ds/symlink/opa462.pdf
另外,在OPA462的产品主页上也提供了TINA reference model,您可以根据您的应用需求仿真下,看是否能满足 要求。