This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540的Center查找特征失败



我把center和peripheral的GATTProfile文件修改成char1能发送20个字节,错误。

if ( pMsg->method == ATT_READ_BY_TYPE_RSP &&
      pMsg->msg.readByTypeRsp.numPairs > 0 ) {
    simpleBLECharHdl = BUILD_UINT16( pMsg->msg.readByTypeRsp.dataList[0],
                                     pMsg->msg.readByTypeRsp.dataList[1] );
    LCD_WRITE_STRING( "Simple Svc Found", HAL_LCD_LINE_1 );
    simpleBLEProcedureInProgress = FALSE;
    simpleBLEDiscState = BLE_DISC_STATE_IDLE;
}

不能进入到上述函数。

我修改的代码为:

 simpleGATTprofile.h

// Profile Parameters
#define SIMPLEPROFILE_CHAR1 0 // RW uint8 - Profile Characteristic 1 value
#define SIMPLEPROFILE_CHAR2 1 // RW uint8 - Profile Characteristic 2 value

// Simple Profile Service UUID
#define SIMPLEPROFILE_SERV_UUID 0xFFF0

// Key Pressed UUID
#define SIMPLEPROFILE_CHAR1_UUID 0xFFF1
#define SIMPLEPROFILE_CHAR2_UUID 0xFFF2

// Simple Keys Profile Services bit fields
#define SIMPLEPROFILE_SERVICE 0x00000001

#define SIMPLEPROFILE_CHAR1_LEN 20

 simpleGATTprofile.c

/*********************************************************************
 * CONSTANTS
 */

#define SERVAPP_NUM_ATTR_SUPPORTED        8

/*********************************************************************
 * TYPEDEFS
 */

/*********************************************************************
 * GLOBAL VARIABLES
 */
// Simple GATT Profile Service UUID: 0xFFF0
CONST uint8 simpleProfileServUUID[ATT_BT_UUID_SIZE] =
{
  LO_UINT16(SIMPLEPROFILE_SERV_UUID), HI_UINT16(SIMPLEPROFILE_SERV_UUID)
};

// Characteristic 1 UUID: 0xFFF1
CONST uint8 simpleProfilechar1UUID[ATT_BT_UUID_SIZE] =
{
  LO_UINT16(SIMPLEPROFILE_CHAR1_UUID), HI_UINT16(SIMPLEPROFILE_CHAR1_UUID)
};

// Characteristic 2 UUID: 0xFFF2
CONST uint8 simpleProfilechar2UUID[ATT_BT_UUID_SIZE] =
{
  LO_UINT16(SIMPLEPROFILE_CHAR2_UUID), HI_UINT16(SIMPLEPROFILE_CHAR2_UUID)
};

/*********************************************************************
 * EXTERNAL VARIABLES
 */

/*********************************************************************
 * EXTERNAL FUNCTIONS
 */

/*********************************************************************
 * LOCAL VARIABLES
 */

static simpleProfileCBs_t *simpleProfile_AppCBs = NULL;

/*********************************************************************
 * Profile Attributes - variables
 */

// Simple Profile Service attribute
static CONST gattAttrType_t simpleProfileService = { ATT_BT_UUID_SIZE, simpleProfileServUUID };


// Simple Profile Characteristic 1 Properties
static uint8 simpleProfileChar1Props = GATT_PROP_READ | GATT_PROP_WRITE;

// Characteristic 1 Value
static uint8 simpleProfileChar1[SIMPLEPROFILE_CHAR1_LEN] =/*{0} ;*/ /**/{0xFC,0x02,0x03,0x05,0xDE,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};/**/

// Simple Profile Characteristic 1 User Description
static uint8 simpleProfileChar1UserDesp[17] = "Characteristic 1\0";



// Simple Profile Characteristic 2 Properties
static uint8 simpleProfileChar2Props = GATT_PROP_NOTIFY;

// Characteristic 2 Value
static uint8 simpleProfileChar2 = 0;

// Simple Profile Characteristic 2 Configuration Each client has its own
// instantiation of the Client Characteristic Configuration. Reads of the
// Client Characteristic Configuration only shows the configuration for
// that client and writes only affect the configuration of that client.
static gattCharCfg_t simpleProfileChar2Config[GATT_MAX_NUM_CONN];

// Simple Profile Characteristic 2 User Description
static uint8 simpleProfileChar2UserDesp[17] = "Characteristic 2\0";



/*********************************************************************
 * Profile Attributes - Table
 */

static gattAttribute_t simpleProfileAttrTbl[SERVAPP_NUM_ATTR_SUPPORTED] =
{
  // Simple Profile Service
  {
    { ATT_BT_UUID_SIZE, primaryServiceUUID }, /* type */
    GATT_PERMIT_READ,                         /* permissions */
    0,                                        /* handle */
    (uint8 *)&simpleProfileService            /* pValue */
  },

    // Characteristic 1 Declaration
    {
      { ATT_BT_UUID_SIZE, characterUUID },
      GATT_PERMIT_READ,
      0,
      &simpleProfileChar1Props
    },

      // Characteristic Value 1
      {
        { ATT_BT_UUID_SIZE, simpleProfilechar1UUID },
        GATT_PERMIT_READ | GATT_PERMIT_WRITE,
        0,
        simpleProfileChar1
      },

      // Characteristic 1 User Description
      {
        { ATT_BT_UUID_SIZE, charUserDescUUID },
        GATT_PERMIT_READ,
        0,
        simpleProfileChar1UserDesp
      },


    // Characteristic 2 Declaration
    {
      { ATT_BT_UUID_SIZE, characterUUID },
      GATT_PERMIT_READ,
      0,
      &simpleProfileChar2Props
    },

      // Characteristic Value 2
      {
        { ATT_BT_UUID_SIZE, simpleProfilechar2UUID },
        0,
        0,
        &simpleProfileChar2
      },

      // Characteristic 2 configuration
      {
        { ATT_BT_UUID_SIZE, clientCharCfgUUID },
        GATT_PERMIT_READ | GATT_PERMIT_WRITE,
        0,
        (uint8 *)simpleProfileChar2Config
      },

      // Characteristic 2 User Description
      {
        { ATT_BT_UUID_SIZE, charUserDescUUID },
        GATT_PERMIT_READ,
        0,
        simpleProfileChar2UserDesp
      },

};


/*********************************************************************
 * LOCAL FUNCTIONS
 */
static uint8 simpleProfile_ReadAttrCB( uint16 connHandle, gattAttribute_t *pAttr,
                            uint8 *pValue, uint8 *pLen, uint16 offset, uint8 maxLen );
static bStatus_t simpleProfile_WriteAttrCB( uint16 connHandle, gattAttribute_t *pAttr,
                                 uint8 *pValue, uint8 len, uint16 offset );

static void simpleProfile_HandleConnStatusCB( uint16 connHandle, uint8 changeType );


/*********************************************************************
 * PROFILE CALLBACKS
 */
// Simple Profile Service Callbacks
CONST gattServiceCBs_t simpleProfileCBs =
{
  simpleProfile_ReadAttrCB,  // Read callback function pointer
  simpleProfile_WriteAttrCB, // Write callback function pointer
  NULL                       // Authorization callback function pointer
};

/*********************************************************************
 * PUBLIC FUNCTIONS
 */

/*********************************************************************
 * @fn      SimpleProfile_AddService
 *
 * @brief   Initializes the Simple Profile service by registering
 *          GATT attributes with the GATT server.
 *
 * @param   services - services to add. This is a bit map and can
 *                     contain more than one service.
 *
 * @return  Success or Failure
 */
bStatus_t SimpleProfile_AddService( uint32 services )
{
  uint8 status = SUCCESS;

  // Initialize Client Characteristic Configuration attributes
  GATTServApp_InitCharCfg( INVALID_CONNHANDLE, simpleProfileChar2Config );

  // Register with Link DB to receive link status change callback
  VOID linkDB_Register( simpleProfile_HandleConnStatusCB );

  if ( services & SIMPLEPROFILE_SERVICE )
  {
    // Register GATT attribute list and CBs with GATT Server App
    status = GATTServApp_RegisterService( simpleProfileAttrTbl,
                                          GATT_NUM_ATTRS( simpleProfileAttrTbl ),
                                          &simpleProfileCBs );
  }

  return ( status );
}


/*********************************************************************
 * @fn      SimpleProfile_RegisterAppCBs
 *
 * @brief   Registers the application callback function. Only call
 *          this function once.
 *
 * @param   callbacks - pointer to application callbacks.
 *
 * @return  SUCCESS or bleAlreadyInRequestedMode
 */
bStatus_t SimpleProfile_RegisterAppCBs( simpleProfileCBs_t *appCallbacks )
{
  if ( appCallbacks )
  {
    simpleProfile_AppCBs = appCallbacks;

    return ( SUCCESS );
  }
  else
  {
    return ( bleAlreadyInRequestedMode );
  }
}


/*********************************************************************
 * @fn      SimpleProfile_SetParameter
 *
 * @brief   Set a Simple Profile parameter.
 *
 * @param   param - Profile parameter ID
 * @param   len - length of data to right
 * @param   value - pointer to data to write.  This is dependent on
 *          the parameter ID and WILL be cast to the appropriate
 *          data type (example: data type of uint16 will be cast to
 *          uint16 pointer).
 *
 * @return  bStatus_t
 */
bStatus_t SimpleProfile_SetParameter( uint8 param, uint8 len, void *value )
{
  bStatus_t ret = SUCCESS;
  switch ( param )
  {
    case SIMPLEPROFILE_CHAR1:
      if ( len <= SIMPLEPROFILE_CHAR1_LEN )
      {
          VOID osal_memcpy( simpleProfileChar1, value, len );
      }
      else
      {
        ret = bleInvalidRange;
      }
      break;

    case SIMPLEPROFILE_CHAR2:
      if ( len == sizeof ( uint8 ) )
      {
        simpleProfileChar2 = *((uint8*)value);

        // See if Notification has been enabled
        GATTServApp_ProcessCharCfg( simpleProfileChar2Config, &simpleProfileChar2, FALSE,
                                    simpleProfileAttrTbl, GATT_NUM_ATTRS( simpleProfileAttrTbl ),
                                    INVALID_TASK_ID );
      }
      else
      {
        ret = bleInvalidRange;
      }
      break;

    default:
      ret = INVALIDPARAMETER;
      break;
  }

  return ( ret );
}

/*********************************************************************
 * @fn      SimpleProfile_GetParameter
 *
 * @brief   Get a Simple Profile parameter.
 *
 * @param   param - Profile parameter ID
 * @param   value - pointer to data to put.  This is dependent on
 *          the parameter ID and WILL be cast to the appropriate
 *          data type (example: data type of uint16 will be cast to
 *          uint16 pointer).
 *
 * @return  bStatus_t
 */
bStatus_t SimpleProfile_GetParameter( uint8 param, void *value )
{
  bStatus_t ret = SUCCESS;
  switch ( param )
  {
    case SIMPLEPROFILE_CHAR1:
	   VOID osal_memcpy( value, simpleProfileChar1, SIMPLEPROFILE_CHAR1_LEN );  //simpleProfileChar1 是数组名
      break;

    case SIMPLEPROFILE_CHAR2:
      *((uint8*)value) = simpleProfileChar2;
      break;

    default:
      ret = INVALIDPARAMETER;
      break;
  }

  return ( ret );
}

/*********************************************************************
 * @fn          simpleProfile_ReadAttrCB
 *
 * @brief       Read an attribute.
 *
 * @param       connHandle - connection message was received on
 * @param       pAttr - pointer to attribute
 * @param       pValue - pointer to data to be read
 * @param       pLen - length of data to be read
 * @param       offset - offset of the first octet to be read
 * @param       maxLen - maximum length of data to be read
 *
 * @return      Success or Failure
 */
static uint8 simpleProfile_ReadAttrCB( uint16 connHandle, gattAttribute_t *pAttr,
                            uint8 *pValue, uint8 *pLen, uint16 offset, uint8 maxLen )
{
  bStatus_t status = SUCCESS;

  // If attribute permissions require authorization to read, return error
  if ( gattPermitAuthorRead( pAttr->permissions ) )
  {
    // Insufficient authorization
    return ( ATT_ERR_INSUFFICIENT_AUTHOR );
  }

  // Make sure it's not a blob operation (no attributes in the profile are long)
  if ( offset > 0 )
  {
    return ( ATT_ERR_ATTR_NOT_LONG );
  }

  if ( pAttr->type.len == ATT_BT_UUID_SIZE )
  {
    // 16-bit UUID
    uint16 uuid = BUILD_UINT16( pAttr->type.uuid[0], pAttr->type.uuid[1]);
    switch ( uuid )
    {
      case SIMPLEPROFILE_CHAR1_UUID:
        *pLen = SIMPLEPROFILE_CHAR1_LEN;
        VOID osal_memcpy( pValue, pAttr->pValue, SIMPLEPROFILE_CHAR1_LEN );
        break;
      case SIMPLEPROFILE_CHAR2_UUID:
        *pLen = 1;
        pValue[0] = *pAttr->pValue;
        break;

      default:
        // Should never get here! (characteristics 3 and 4 do not have read permissions)
        *pLen = 0;
        status = ATT_ERR_ATTR_NOT_FOUND;
        break;
    }
  }
  else
  {
    // 128-bit UUID
    *pLen = 0;
    status = ATT_ERR_INVALID_HANDLE;
  }

  return ( status );
}

/*********************************************************************
 * @fn      simpleProfile_WriteAttrCB
 *
 * @brief   Validate attribute data prior to a write operation
 *
 * @param   connHandle - connection message was received on
 * @param   pAttr - pointer to attribute
 * @param   pValue - pointer to data to be written
 * @param   len - length of data
 * @param   offset - offset of the first octet to be written
 * @param   complete - whether this is the last packet
 * @param   oper - whether to validate and/or write attribute value
 *
 * @return  Success or Failure
 */

static bStatus_t simpleProfile_WriteAttrCB( uint16 connHandle, gattAttribute_t *pAttr,
                                 uint8 *pValue, uint8 len, uint16 offset )

{
  bStatus_t status = SUCCESS;
  uint8 notifyApp = 0xFF;

  // If attribute permissions require authorization to write, return error
  if ( gattPermitAuthorWrite( pAttr->permissions ) )
  {
    // Insufficient authorization
    return ( ATT_ERR_INSUFFICIENT_AUTHOR );
  }

  if ( pAttr->type.len == ATT_BT_UUID_SIZE )
  {
    // 16-bit UUID
    uint16 uuid = BUILD_UINT16( pAttr->type.uuid[0], pAttr->type.uuid[1]);
    switch ( uuid )
    {
      case SIMPLEPROFILE_CHAR1_UUID:

        //Validate the value
        // Make sure it's not a blob oper
        if ( offset == 0 )
        {
            if ( len > SIMPLEPROFILE_CHAR1_LEN )
            {
                status = ATT_ERR_INVALID_VALUE_SIZE;
            }
        }
        else
        {
          status = ATT_ERR_ATTR_NOT_LONG;
        }

        //Write the value
        if ( status == SUCCESS )
        {
//            uint8 *pCurValue = (uint8 *)pAttr->pValue;
//            osal_memset(pCurValue,0,SIMPLEPROFILE_CHAR1_LEN);
//            VOID osal_memcpy( pCurValue, pValue, len );

            uint8 i = 0;
            uint8 *pCurValue = (uint8 *)pAttr->pValue;
            for ( i = 0; i<len; i++) {
                *pCurValue = pValue[i];
                pCurValue++;
            };
            if(len < SIMPLEPROFILE_CHAR1_LEN) {
                for (; i<SIMPLEPROFILE_CHAR1_LEN; i++) {
                    *pCurValue = 0;
                    *pCurValue ++;
                }
            }
            notifyApp = SIMPLEPROFILE_CHAR1;
        }
        break;

      case GATT_CLIENT_CHAR_CFG_UUID:
        status = GATTServApp_ProcessCCCWriteReq( connHandle, pAttr, pValue, len,
                                                 offset, GATT_CLIENT_CFG_NOTIFY );
        break;

      default:
        // Should never get here! (characteristics 2 and 4 do not have write permissions)
        status = ATT_ERR_ATTR_NOT_FOUND;
        break;
    }
  }
  else
  {
    // 128-bit UUID
    status = ATT_ERR_INVALID_HANDLE;
  }

  // If a charactersitic value changed then callback function to notify application of change
  if ( (notifyApp != 0xFF ) && simpleProfile_AppCBs && simpleProfile_AppCBs->pfnSimpleProfileChange )
  {
    simpleProfile_AppCBs->pfnSimpleProfileChange( notifyApp );  //调用回调函数 simpleProfileChangeCB()
  }

  return ( status );
}


/*********************************************************************
 * @fn          simpleProfile_HandleConnStatusCB
 *
 * @brief       Simple Profile link status change handler function.
 *
 * @param       connHandle - connection handle
 * @param       changeType - type of change
 *
 * @return      none
 */
static void simpleProfile_HandleConnStatusCB( uint16 connHandle, uint8 changeType )
{
  // Make sure this is not loopback connection
  if ( connHandle != LOOPBACK_CONNHANDLE )
  {
    // Reset Client Char Config if connection has dropped
    if ( ( changeType == LINKDB_STATUS_UPDATE_REMOVED )      ||
         ( ( changeType == LINKDB_STATUS_UPDATE_STATEFLAGS ) &&
           ( !linkDB_Up( connHandle ) ) ) )
    {
      GATTServApp_InitCharCfg( connHandle, simpleProfileChar2Config );
    }
  }
}

 
具体的两个文件就修改成这样,好奇怪就是不行。后开我修改了simpleProfile_ReadAttrCB函数的:
      case SIMPLEPROFILE_CHAR1_UUID:
        *pLen = SIMPLEPROFILE_CHAR1_LEN;
        VOID osal_memcpy( pValue, pAttr->pValue, SIMPLEPROFILE_CHAR1_LEN );
        break;

改成:

      case SIMPLEPROFILE_CHAR1_UUID:
          *pLen = 16;
          VOID osal_memcpy( pValue, pAttr->pValue, SIMPLEPROFILE_CHAR1_LEN );
          break;

这就可以了。不明白为什么。

 

 
  • 我查找特征部分代码:

    static void simpleBLEGATTDiscoveryEvent( gattMsgEvent_t *pMsg )
    {
        attReadByTypeReq_t req;
    
        if ( simpleBLEDiscState == BLE_DISC_STATE_SVC ) {
            // Service found, store handles      //当通过uuid GATT_DiscPrimaryServiceByUUID() 调用成功
            if ( pMsg->method == ATT_FIND_BY_TYPE_VALUE_RSP &&
                 pMsg->msg.findByTypeValueRsp.numInfo > 0 ) {
                simpleBLESvcStartHdl = pMsg->msg.findByTypeValueRsp.handlesInfo[0].handle;
                simpleBLESvcEndHdl = pMsg->msg.findByTypeValueRsp.handlesInfo[0].grpEndHandle;
            }
            // If procedure complete
            if ( ( pMsg->method == ATT_FIND_BY_TYPE_VALUE_RSP  &&
                   pMsg->hdr.status == bleProcedureComplete ) ||
                 ( pMsg->method == ATT_ERROR_RSP ) )  {
                if ( simpleBLESvcStartHdl != 0 ) {
                    // Discover characteristic
                    simpleBLEDiscState = BLE_DISC_STATE_CHAR;
                    req.startHandle = simpleBLESvcStartHdl;
                    req.endHandle = simpleBLESvcEndHdl;
                    req.type.len = ATT_BT_UUID_SIZE;
                    req.type.uuid[0] = LO_UINT16(SIMPLEPROFILE_CHAR1_UUID);
                    req.type.uuid[1] = HI_UINT16(SIMPLEPROFILE_CHAR1_UUID);
                    GATT_ReadUsingCharUUID( simpleBLEConnHandle, &req, simpleBLETaskId );  //根据服务的UUID调用API函数GATT_ReadUsingCharUUID协议栈会返回该服务的Handle。
                }
            }
        } else if ( simpleBLEDiscState == BLE_DISC_STATE_CHAR ) {
            if ( pMsg->method == ATT_READ_BY_TYPE_RSP &&
                 pMsg->msg.readByTypeRsp.numPairs > 0 ) {
                simpleBLECharHdl = BUILD_UINT16( pMsg->msg.readByTypeRsp.dataList[0],
                                                 pMsg->msg.readByTypeRsp.dataList[1] );
                LCD_WRITE_STRING( "Simple Svc Found11", HAL_LCD_LINE_1 );
                simpleBLEProcedureInProgress = FALSE;
                simpleBLEDiscState = BLE_DISC_STATE_IDLE;
            }else {
                simpleBLEDiscState = BLE_DISC_STATE_CHAR2;
                req.startHandle = simpleBLESvcStartHdl;
                req.endHandle = simpleBLESvcEndHdl;
                req.type.len = ATT_BT_UUID_SIZE;
                req.type.uuid[0] = LO_UINT16(SIMPLEPROFILE_CHAR2_UUID);    //获取特性值xxxxx的handle
                req.type.uuid[1] = HI_UINT16(SIMPLEPROFILE_CHAR2_UUID);
                GATT_ReadUsingCharUUID( simpleBLEConnHandle, &req, simpleBLETaskId );
            }
        }else if ( simpleBLEDiscState == BLE_DISC_STATE_CHAR2 ) {
            if ( pMsg->method == ATT_READ_BY_TYPE_RSP &&
                 pMsg->msg.readByTypeRsp.numPairs > 0 ) {
                simpleBLECharHdl2 = BUILD_UINT16( pMsg->msg.readByTypeRsp.dataList[0],
                                                  pMsg->msg.readByTypeRsp.dataList[1] );
                LCD_WRITE_STRING( "Simple Svc Found22", HAL_LCD_LINE_1 );
                simpleBLEProcedureInProgress = FALSE;
                LCD_WRITE_STRING( "0000000", HAL_LCD_LINE_8 );
    
                attWriteReq_t AttReq;
                uint8 ValueBuf[2];
                AttReq.handle = simpleBLECharHdl2;
                AttReq.len = 2;
                AttReq.sig = 0;
                AttReq.cmd = 0;
                ValueBuf[0] = 0x01;
                ValueBuf[1] = 0x00;
                osal_memcpy(AttReq.value,ValueBuf,2);
                GATT_WriteCharValue( 0, &AttReq, simpleBLETaskId );
            }
            simpleBLEDiscState = BLE_DISC_STATE_IDLE;
        }
    }
    

    他死活不能查找成功。