This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2540 Timer3 通道1输出比较模式产生PWM波

Other Parts Discussed in Thread: CC2540

大家好,我想用cc2540定时器3的通道1的输出比较模式产生38kHz的PWM波,程序如下。但是通道1始终输出高电平,请各位解答,谢谢!

#include<ioCC2540.h>

typedef unsigned char uint8;

#define BV(x) (1<<(x))

void InitTimer3()
{

T3CTL=0x2A;
                                 //溢出中断
                                 //2分频,8M
                                 //modulo mode
T3CC0=0xD2;
T3CC1=0x46;            //38kHz,33%占空比
PERCFG |= BV(5);   
T3CCTL1=0x64;
                                    //通道1设置
P1DIR |= BV(7);
P1SEL |= BV(7);      //p1.7外设,输出
T3CTL |= BV(4);      //start timer3
T3IE=1;
EA=1;                       //开启中断

}

#pragma vector = T3_VECTOR
__interrupt void Timer3_ISR(void)
{
IRCON=0x00;
}

void main(void)
{

InitTimer3();

while(1)
{  }
}