求救:CC2650 Launchpad 板载XDS110的驱动问题,ccs一直提示报错,需要升级驱动
(1) 如下图所示,XDS110的驱动是安装好的。
(2)但是用CCS 6.2 点击debug后,就报错提示,如下图
(3) 点击“Update”后CCS死机,设备管理器的设备变成如下图所示。
(4)我的驱动如下图,应该没问题吧
(5) 急求高手帮忙,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求救:CC2650 Launchpad 板载XDS110的驱动问题,ccs一直提示报错,需要升级驱动
(1) 如下图所示,XDS110的驱动是安装好的。
(2)但是用CCS 6.2 点击debug后,就报错提示,如下图
(3) 点击“Update”后CCS死机,设备管理器的设备变成如下图所示。
(4)我的驱动如下图,应该没问题吧
(5) 急求高手帮忙,谢谢!
装个CCS7吧,或者 最新的flashprogrammer2
http://www.ti.com/tool/flash-programmer
SmartRF Flash Programmer 2 can be used to program the flash memory in Texas Instruments ARM based low-power RF wireless MCUs over the debug and serial interfaces.
SmartRF Flash Programmer can be used to program the flash memory in Texas Instruments 8051-based low-power RF wireless MCUs and for upgrading the firmware and bootloader on the SmartRF05 Evaluation Board, SmartRF Transceiver Evaluation Board (TrxEB) and the CC-Debugger.
The SmartRF Flash Programmer and SmartRF Flash Programmer 2 both include a graphical user interface and a command line interface.
SmartRF Flash Programmer and SmartRF Flash Programmer 2 run on 32 and 64-bit versions of Microsoft® Windows 7 and Windows 8.
或者smartstudio,这些软件也都能识别xds110,并提示升级固件
http://www.ti.com/tool/smartrftm-studio
| Part Number | Buy from Texas Instruments or Third Party | Alert Me | Status | Current Version | Version Date |
SMARTRFTM-STUDIO:
|
Free |
ACTIVE | 2.6.0 | 09-MAR-2017 |
SmartRF™ Studio is a Windows application that can be used to evaluate and configure Low Power RF devices from Texas Instruments. The application will help designers of RF systems to easily evaluate the radio at an early stage in the design process. It is especially useful for generation of configuration register values and for practical testing and debugging of the RF system. SmartRF Studio can be used either as a standalone application or together with applicable evaluation boards or debug probes for the RF device.
SmartRF™ Studio supports all the Low Power RF devices from TI. Note that you might need to use an older version of the tool to work with some of the older devices.
SmartRF Studio 6
SmartRF Studio 7
SmartRF Studio 6 runs on Microsoft® Windows 98, Windows 2000, Windows XP (32 bit), Windows Vista (32 bit) and Windows 7 (32 bit).
SmartRF Studio 7 runs on 32 and 64-bit versions of Microsoft® Windows 7, 8 and 10.
Installation Recommendations: