Other Parts Discussed in Thread: CC2564C
我参考书册,自己画的板子,用的CC2564C,在蓝牙连接时不稳定,总共做了7块,有三块连接很好,其它几块连接不好,现象如下:
1.所有均能接收广播,RSSI的值没有明显差异;
2.连接不好的板子,在将被连接设备紧靠板子时,较容易连接,但是过一段时间后会断开,错误码是Connection Timeout (0x08);
3.曾经怀疑是26MHz的晶体的时钟电路有频偏,故更换过电容,刚换完在电路板CC2564C、晶体、电容、天线区域由于加热温度较高还没有完全冷却时,此时通电所有连接不好的板子均能非常正常的连接;
4.由于连接不稳定,我在软件上加了重连和CC2564C复位重连的机制,但是仍然不能解决连接不好的问题,经常出现刚收到LE connection complete事件就立马收到连接断开事件,错误码是Connection Failed To Be Established (0x3E)。
PS:用的26MHz晶体,陶瓷天线,巴伦用的手册推荐的,靠近板边放置。我直接用的HCI底层command连接,没用使用协议栈。
请问各位,是否遇到过类似问题,是我26MHz时钟的频偏,还是天线部分的问题(连接情况受两个设备的距离影响),我已经更换过不同26MHz晶体、不同容值的电容,天线了,均没有太大变化,实在是没有办法了,手里也没有频谱分析测试设备。