Other Parts Discussed in Thread: CC2540
1.采用了TI的参考设计,集成巴伦方案,设置输出功率为4dbm,我们测出来大部分在3dbm多一点,这是正常的。但是有一块是5.2dbm,这会是芯片的差异吗
我看CC2540的datasheet 最大输出功率的typ为4dbm,没有写MAX和MIN值
2.在DTM测试模式下,RX GAIN是高增益模式吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2540
1.采用了TI的参考设计,集成巴伦方案,设置输出功率为4dbm,我们测出来大部分在3dbm多一点,这是正常的。但是有一块是5.2dbm,这会是芯片的差异吗
我看CC2540的datasheet 最大输出功率的typ为4dbm,没有写MAX和MIN值
2.在DTM测试模式下,RX GAIN是高增益模式吗
Hank Zhang 说:1.采用了TI的参考设计,集成巴伦方案,设置输出功率为4dbm,我们测出来大部分在3dbm多一点,这是正常的。但是有一块是5.2dbm,这会是芯片的差异吗
我看CC2540的datasheet 最大输出功率的typ为4dbm,没有写MAX和MIN值
2.在DTM测试模式下,RX GAIN是高增益模式吗
1. 从规格书看的话,没问题。但是,如果你要是要debug的话,可以做一下交叉测试。看看问题是跟着芯片还是balun走。
2. RX gain是自动的。会根据RSSI调整的。信号如果弱,肯定是high gain.
BR. AZ