This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2540/cc2541 debug mode

所以,debugmode要如何关闭呢

  • 3.1 Debug Mode
    Debug mode is entered by forcing two falling-edge transitions on pin P2.2 (debug clock) while the RESET_N input is held low. When RESET_N is set high, the device is in debug mode.
    On entering debug mode, the CPU is in the halted state with the program counter reset to address 0x0000.
    While in debug mode, pin P2.1 is the debug-data bidirectional pin, and P2.2 is the debug-clock input pin

    上电时不做上述操作就不会进入debug mode,更多内容请参考:www.ti.com/.../swru191f.pdf