This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P 如果脱机运行?

Other Parts Discussed in Thread: UNIFLASH, CC1352P

TI专家:

          我现在使用的是CC13X2P_4_LAUNCHX板子,CCS是9.3 SDK是simplelink_cc13x2_26x2_sdk_3_40_00_02 ,我导入project_zero_app_CC13X2P_4_LAUNCHXL_tirtos_ccs这个项目,发现脱机时无法运行,之前已经发帖求助过,我看了之前别人同样问题的贴子,感觉越看越糊涂。我明白我现在的问题是bootloader没有运行正确,或者是烧录的不正确。

           

  • 请问:
    1、不脱机是否运行正常?
    2、您是否把文件烧录进板子?
  • TI专家:
    我仔细观看了dev.ti.com/.../node
    仔细观看project_zero_app_CC13X2P_4_LAUNCHXL_tirtos_ccs编译过程中其实已经调用这个工具了oad_image_tool
    C:/ti/simplelink_cc13x2_26x2_sdk_3_40_00_02/tools/common/oad/oad_image_tool --verbose ccs D:/CCS_workspace_v9/project_zero_app_CC13X2P_4_LAUNCHXL_tirtos_ccs 7 -hex1 Release/project_zero_app_CC13X2P_4_LAUNCHXL_tirtos_ccs.hex -k C:/ti/simplelink_cc13x2_26x2_sdk_3_40_00_02/tools/common/oad/private.pem -o Release/project_zero_app_CC13X2P_4_LAUNCHXL_tirtos_ccs_oad

    编译后产生三个文件,project_zero_app_CC13X2P_4_LAUNCHXL_tirtos_ccs.hex
    project_zero_app_CC13X2P_4_LAUNCHXL_tirtos_ccs_oad.bin
    sign.bin
    但是我使用UniFlash烧录这些文件板子是没法正常运行。
  • 谢谢!
    在Debug 或者是Release模式下运行一直都是正常的。
  • 您好,您发的链接无法打开,如果是要验证project zero,建议看这个academy:dev.ti.com/.../node

    一步步操作,看卡在哪一步
  • TI 专家:
    谢谢你的支持,我按照你的说明做到第二个任务的时候,就出现异常了。在手机端不能发现Project Zero这个设备,但是串口信息没有发现异常。我把设备人为复位后,打印以下信息:
    #000001 [ 0.031 ] [32;1mINFO: [30;1m(led_service.c:221) [0mRegistered service, 5 attributes, status 0x00

    #000002 [ 0.031 ] [32;1mINFO: [30;1m(button_service.c:260) [0mRegistered service, 7 attributes

    #000003 [ 0.031 ] [32;1mINFO: [30;1m(data_service.c:239) [0mRegistered service, 6 attributes

    #000004 [ 6.026 ] [32;1mINFO: [30;1m(project_zero.c:632) [0mRegistered OAD Service

    #000005 [ 6.026 ] [32;1mINFO: [30;1m(project_zero.c:2932) [0mLeft button not held under boot, not reverting to factory.

    #000006 [ 6.026 ] [32;1mINFO: [30;1m(project_zero.c:2934) [0mRight+Left button not held under boot, not erasing external flash.

    #000007 [ 6.026 ] [32;1mINFO: [30;1m(project_zero.c:650) [0mOAD Image v0002

    #000008 [ 6.026 ] [32;1mINFO: [30;1m(led_service.c:237) [0mRegistered callbacks to application. Struct @20001b6c

    #000009 [ 6.026 ] [32;1mINFO: [30;1m(button_service.c:278) [0mRegistered callbacks to application. Struct @20001b74

    #000010 [ 6.026 ] [32;1mINFO: [30;1m(data_service.c:257) [0mRegistered callbacks to application. Struct @20001b7c

    #000011 [ 6.026 ] [32;1mINFO: [30;1m(led_service.c:272) [0mSetParameter : LED0 len: 1

    #000012 [ 6.026 ] [32;1mINFO: [30;1m(led_service.c:280) [0mSetParameter : LED1 len: 1

    #000013 [ 6.026 ] [32;1mINFO: [30;1m(button_service.c:319) [0mSetParameter : BUTTON0 len: 1

    #000014 [ 6.026 ] [32;1mINFO: [30;1m(button_service.c:352) [0mTrying to send noti/ind: connHandle ffff, [33mNoti/ind disabled[0m

    #000015 [ 6.026 ] [32;1mINFO: [30;1m(button_service.c:330) [0mSetParameter : BUTTON1 len: 1

    #000016 [ 6.026 ] [32;1mINFO: [30;1m(button_service.c:352) [0mTrying to send noti/ind: connHandle ffff, [33mNoti/ind disabled[0m

    #000017 [ 6.026 ] [32;1mINFO: [30;1m(data_service.c:295) [0mSetParameter : String len: 40

    #000018 [ 6.026 ] [32;1mINFO: [30;1m(data_service.c:306) [0mSetParameter : Stream len: 20

    #000019 [ 6.026 ] [32;1mINFO: [30;1m(data_service.c:328) [0mTrying to send noti/ind: connHandle ffff, [33mNoti/ind disabled[0m

    #000020 [ 6.032 ] [32;1mINFO: [30;1m(project_zero.c:1160) [0mGAP is started. Our address: [32m04:EE:03:4C:08:ED[0m

    #000021 [ 6.032 ] [32;1mINFO: [30;1m(project_zero.c:1175) [0mName in advData1 array: [33mProject Zero[0m

    #000022 [ 6.039 ] [32;1mINFO: [30;1m(project_zero.c:1398) [0mAdv Set 0 Enabled
  • TI专家:
    cc13x2p4lp_bim_offchip这个项目我没有做修改,Project Zero项目我修改为支持蓝牙4.2版本。
    我重新烧录一个 pinStandby项目,破坏掉bootloader,这时再烧录Project Zero项目就可以在手机端发现 Project Zero设备,手机端操作没有问题,当然脱机复位后就不能再次运行了。
  • 我刚才用板子操作了一下,复位以后可以运行,而且我手机用BLE scanner搜索并连接到了project zero

  • 用flash programmer把这两个hex文件烧录进去再试试

  • 谢谢 TI专家 !
    帖子回复的比较晚了,同样的固件我在自己设计的板子上可以正常运行,但是在CC1352P4开发板上不能正常运行。
    但是C11352P是我前几天刚刚跟新到最新的芯片,我后续再换一片芯片试试。
  • 不客气,期待你的好消息

  • TI专家:
    今天新的IC到货,更换CC1352P E后,开发板可以正常使用了。谢谢你的支持!