关于STM32F4平台下的cc2564C的HIDDemo(鼠标例子)C:\TI\Connectivity\CC256X BT\CC256x STM32 Bluetopia SDK\v4.0.2.2\NoOS\STM3240G-EVAL\Samples\HIDDemo例程,测试发现蓝牙协议栈初始化成功,但是用手机端测试无法连接蓝牙,请问这个怎么解决呢,我现在想把这个例程改程HID Keyboard,请问有没有相关例子参考的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Bluetooth Stack ID: 1
Device Chipset: 4.1
BTPS Version : 4.0.2.1
Project Type : 6
FW Version : 12.26
App Name : HIDDemo
App Version : 0.2
LOCAL BD_ADDR: 0x88C255D1D711
GAP_Set_Connectability_Mode(cmConnectable).
GAP_Set_Discoverability_Mode(dmGeneralDiscoverable, 0).
GAP_Set_Pairability_Mode(pmPairableMode).
GAP_Register_Remote_Authentication() Success.
************************** Command Options **************************
* Command Options: Host, Device *
*********************************************************************
Select Mode>Device
HID_Register_Device_Server: Function Successful.
HID_Register_Device_SDP_Record: Function Successful.
这个是初始化后串口打印的信息,打印出信息之后,我用手机搜索,搜索不到蓝牙,我的目的是想把这个例程改程HID Keyboard,你们这边是否可以给一些建议,我如何修改