Other Parts Discussed in Thread: CC2541, TPS62730
你好,我在蓝牙CC2541的电路设计中使用了TPS62730,然后软件上用的是蓝牙1.3.2的协议栈,ON/BYP脚接到P0_7上,在软件中开启了DC_DC_P0_7宏,也使用了POWER_SAVING宏。
用干电池或者稳压的3.3V的供电都是正常可以工作的。但是用锂电池后,锂电池电压最高为4.2V,会发生芯片不断复位重启的现象。
示波器测量后,发现TPS62730在正常的2.1V的输出电压中,非周期性的会出现极短暂的一次高电压波形(即当前锂电池的电压值)然后又恢复为2.1V。
当我在软件中关闭DC_DC_P0_7宏,自行初始化P0_7始终为输出高电平,则可以启动,电压一直为2.1V,但是蓝牙连接非常困难,连接不上。如果用2节1.5V干电池或者稳压的3.3V电源则没有什么问题。
请问这是什么问题呢?