This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2540+cc2590怎么工作?

Other Parts Discussed in Thread: CC2540, CC2590

PAEN,EN,HGM是不是在开机的时候设定就可以?还是在系统运行的时候会自动修改?

蓝牙芯片是CC2540,一片板是没有CC2590的,一片是带CC2590的,烧录同样的程序,不带CC2590的是可以通过手机搜索到蓝牙设备,带CC2590的搜索不到,

CC2590配置电平为:EN=1;PAEN=0;RXTX=0;HGM=0; 请问问题出在哪里

 

PS:R17=NC,电压3.4V