This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot Extend range of CC2540 by using CC2590



   Recently, in my project, I want to extend the range of CC2540 by using CC2590 orCC2591. May I ask some questions to you? Thanks a lot.

    1. In the BLE4.0 Stack, according to  swra422.pdf, I can find HCI_EXT_ExtendRfRangeCmd() in hci.h, but I can not find hci.c, so where can I find definition of HCI_EXT_ExtendRfRangeCmd()??

   2. Due to special application, we can not connect P1_1 to HGM, P1_2 to PA_EN, P1_3 to EN, we want to connect to P1_1 to PA_EN, P1_4 to EN, P0_7 to HGM, but how and where can I modify the code??

 

thanks you a lot

  • Chunyang,

    you are welcome!

    请看附件。 2590和 2541一起的guide.

  • 您好!我仔细研究过附件中的内容,但是对于以下来个问题,还是不明白,向您请教,希望能得到您的帮助。

      1. 根据swra422.pdf,我能够在hci.h中找到HCI_EXT_ExtendRfRangeCmd()这个函数的声明,但是我找不到hci.c,所以我哪里能够找到HCI_EXT_ExtendRfRangeCmd()这个函数的定义??

       2. 在我们的特定应用下,无法按照swra422.pdf中的说明,将 P1_1 连接到 HGM管脚,P1_2 连接到 PA_EN, P1_3 连接到 EN, 二是想将 P1_1 连接到 PA_EN, P1_4 连接到 EN, P0_7 连接到 HGM,我在哪能够修改管脚的映射关系??

    万分感谢!

    祝好!