This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540+CC2590的PCB制作问题

Other Parts Discussed in Thread: CC2541, CC2590

大家好:

       经过详细查看TI官方提供的CC2541+CC2590的开发板文档,注意到CC2541+CC2590EM的制板参数(压缩包里有一个Readme):

PCB DESCRIPTION:4 LAYER PCB 1.6 MM

     Copper        1   35 um

     Dielectric  1-2   0.175 mm (e.g. 1x Prepreg 7628 AT05 47% Resin)

     Copper        2   18 um

     Dielectric  2-3   1.14 mm (6x 7628M 43% Resin)

     Copper        3   18 um

     Dielectric  3-4   0.175 mm (e.g. 1x Prepreg 7628 AT05 47% Resin)

     Copper        4   35 um

 DE104iML or equivalent substrate (Resin contents around 45%, which gives Er=4.42@2.4GHz, TanD=0.016)

 Dimensions in mil (0.001 inch)

 DOUBLE SIDE SOLDER MASK,

 DOUBLE SIDE SILKSCREEN,

 8 MIL MIN TRACE WIDTH AND 5 MIL MIN ISOLATION.

主要有两个问题

(1)由于TI的PCB是采用CADSTAR制作的,我将其转为Altium Designer所对应的工程项目后,通过查看“层叠管理”,如附件中的图所示,具体每层的参数与readme.txt中的参数不同,而且并没有四层铺铜啊。是什么问题呢?

(2)DE104iML 是一种什么材料啊?在网上查不到,问了几家PCB制造厂也说没听过用过这种材料。请问能否采用其他材料代替?