Other Parts Discussed in Thread: CC2541, CC2540, CC2544
希望通过按键中断唤醒PM3模式下的休眠,但是总是出问题,实现不了。PM2格式通过顶过定时器可以实现,那么可以通过检测一个引脚的电平来实现休眠吗?然后通过按键中断来唤醒休眠,这样可以吗?
据说TI的其他工程里面有这样的例子是吗?是哪个呢?
求大神指点下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PM2 是由系统自动调度进入的, 由OSAL调用HAL层的接口实现. PM2 和 PM3都可以通过外部中断来唤醒。
可以参考之前的讨论帖 http://www.deyisupport.com/question_answer/wireless_connectivity/bluetooth/f/103/t/47722.aspx
cc2541 pm3模式可以移植到cc2540
/***********************************************************************************
Filename: powermode3.c
Description: This software example shows how to properly enter Power Mode 3
and then exit upon Port 0 Interrupt. The SRF05EB LED1 is cleared
before entering Power Mode 3, and then set by the Port 0 ISR.
Hence, the LED1 is ON in Active Mode and OFF in Power Mode 3.
Note: PM2 and PM3 is not supported on the CC2544.
***********************************************************************************/
/***********************************************************************************
* INCLUDES
*/
#include <power_mode.h>
#include <hal_types.h>
// Include Name definitions of individual bits and bit-fields in the CC254x device registers.
#include <ioCC254x_bitdef.h>
// Include device specific file
#if (chip==2541)
#include "ioCC2541.h"
#elif (chip==2543)
#include "ioCC2543.h"
#elif (chip==2545)
#include "ioCC2545.h"
#else
#error "Chip not supported!"
#endif
/***********************************************************************************
* CONSTANTS
*/
// Wait time in Active mode.
#define ACT_MODE_TIME 50000
/***********************************************************************************
* LOCAL VARIABLES
*/
// Variable for active mode duration.
static uint32 __xdata activeModeCnt = 0;
/***********************************************************************************
* LOCAL FUNCTIONS
*/
/***********************************************************************************
* @fn setup_port_interrupt
*
* @brief Function which sets up the Port 0 Interrupt for Power Mode 3 usage.
*
* @param void
*
* @return void
*/
void setup_port_interrupt(void)
{
// Clear Port 0 Interrupt flags.
P0IF = 0;
P0IFG = 0x00;
// Interrupt enable on all pins on port 0.
P0IEN = 0xFF;
// Enable CPU Interrupt for Port 0 (IEN1.P0IE = 1).
P0IE = 1;
// Enable Global Interrupt by setting the (IEN0.EA = 1).
EA = 1;
}
/***********************************************************************************
* @fn port0_isr
*
* @brief Port 0 Interrupt Service Routine, which executes when SRF05EB S1
* (P0_1) is pressed.
*
* @param void
*
* @return void
*/
#pragma vector = P0INT_VECTOR
__interrupt void port0_isr(void)
{
// Note that the order in which the following flags are cleared is important.
// Clear Port 0 Interrupt Flags.
P0IFG = 0x00;
// Clear CPU Interrupt Flag for P0 (IRCON.P0IF = 0).
P0IF = 0;
// Set LED1 to indicate Active Mode.
P1_0 = 1;
}
/***********************************************************************************
* @fn main
*
* @brief Enter Power Mode, exit Power Mode 3 using Port 0 Interrupt.
*
* @param none
*
* @return 0
*/
void main(void)
{
/***************************************************************************
* Setup I/O
*/
// Initialize P1_0 for SRF05EB LED1.
P1SEL &= ~BIT0; // Function as General Purpose I/O.
P1_0 = 1; // LED1 on.
P1DIR |= BIT0; // Output.
// Initialize P0_1 for SRF05EB S1 button.
P0SEL &= ~BIT1; // Function as General Purpose I/O.
P0DIR &= ~BIT1; // Input.
P0INP |= BIT1; // 3-state input.
/***************************************************************************
* Setup interrupt
*
* Setup and enable Port 0 Interrupt, which shall wake-up the SoC from
* Power Mode 3.
*/
setup_port_interrupt();
/***********************************************************************
* Setup powermode
*/
// Set [SLEEPCMD.MODE] to PM3.
SLEEPCMD = (SLEEPCMD & ~SLEEPCMD_MODE) | SLEEPCMD_MODE_PM3;
/* Main Loop, enter/exit Power Mode 3. */
while(1)
{
// Wait some time in Active Mode, and clear LED1 before
// entering Power Mode 3.
for(activeModeCnt = 0; activeModeCnt < ACT_MODE_TIME; activeModeCnt++);
P1_0 = 0;
// Enter powermode
// Sets PCON.IDLE with a 2-byte boundary assembly instruction.
// NOTE: Cache must be enabled (see CM in FCTL).
// This method gives the least current consumption.
EnterSleepModeProcessInterruptsOnWakeup();
}
}
/***********************************************************************************
Copyright 2012 Texas Instruments Incorporated. All rights reserved.
IMPORTANT: Your use of this Software is limited to those specific rights
granted under the terms of a software license agreement between the user
who downloaded the software, his/her employer (which must be your employer)
and Texas Instruments Incorporated (the "License"). You may not use this
Software unless you agree to abide by the terms of the License. The License
limits your use, and you acknowledge, that the Software may not be modified,
copied or distributed unless embedded on a Texas Instruments microcontroller
or used solely and exclusively in conjunction with a Texas Instruments radio
frequency transceiver, which is integrated into your product. Other than for
the foregoing purpose, you may not use, reproduce, copy, prepare derivative
works of, modify, distribute, perform, display or sell this Software and/or
its documentation for any purpose.
YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
PROVIDED 揂S IS?WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL
TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER
LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES
INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE
OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT
OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES
(INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.
Should you have any questions regarding your right to use this Software,
contact Texas Instruments Incorporated at www.TI.com.
***********************************************************************************/
谢谢,大秦正声。但是在协议站上使用这个好像不行啊,我是通过检测P1_6是否置高来确定是否进入休眠,休眠函数就是使用上面的那种,但是按键中断换不起来啊,而且功耗也是1点几mA,没有达到0点即uA啊,请问这是怎么回事啊?