This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540主机不连接、直接读出从机的RSSI值



大家好!

我想实现:主机上电,扫描到(正在广播)的从机后,不连接,直接读出从机的RSSI值,并且移动从机,RSSI值可以改变。请问如何实现?谢谢!

ps:

1、我使用的是1.3版本的协议栈,可以实现主从连接后读取移动中的RSSI值。

2、我现在实现的是:主机上电,自动扫描到(正在广播)的从机后,不连接,直接读出从机的RSSI值;但是移动从机,RSSI值不改变。

修改的是 simpleBLECentral 工程里的 simpleBLECentralEventCB 函数中的

case GAP_DEVICE_INFO_EVENT:

      {

        // if filtering device discovery results based on service UUID

        if ( DEFAULT_DEV_DISC_BY_SVC_UUID == TRUE )

        {

          if ( simpleBLEFindSvcUuid( SIMPLEPROFILE_SERV_UUID,

                                     pEvent->deviceInfo.pEvtData,

                                     pEvent->deviceInfo.dataLen ) )

          {

            simpleBLEAddDeviceInfo( pEvent->deviceInfo.addr, pEvent->deviceInfo.addrType );

            //不连接,扫描后,自动读取从机的RSSI

            int8 newRSSI = -(pEvent->deviceInfo.rssi);

            LCD_WRITE_STRING_VALUE("RSSI -dB:",(uint8)(newRSSI),10,HAL_LCD_LINE_1);

           }

        }

      }

      break;