This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541 传输距离

Other Parts Discussed in Thread: CC2541, CC2540, CC2590

我自己做了个 CC2541的模块,板载天线采用的是 AN043 方案,但是传输有效距离只有 10米左右,现在需要有效距离50米左右,想问板载天线可以实现吗?

  • 关于通讯距离的问题,根据实际情况不同,场地是否足够空旷,干扰性是不是很大等有关系。TI提供了空旷环境下的最远通讯距离:CC2540最大发射功率为0dbm,最大距离100m;CC2540+CC2590做PA, 最大发射功率14dbm,最大距离500m,希望能够参考。

    建议您按照TI的参考设计来进行设计电路板