你好,ti工程师,我安装了CC256XM4BTBLESW-v1.2-Setup,我的keil版本为v4.73,我打开的工程路径为:
C:\TI\Connectivity\CC256X BT\CC256x M4 Bluetopia SDK\v1.2\Cortex_M4\Sample\A2DPDemo\NoOS\RVMDK
编译时出现如下错误:
1、
..\..\..\..\Bluetopia\btpskrnl\NoOS\BKRNLAPI.h(28): error: #5: cannot open source input file "utils/ustdlib.h": No such file or directory
2、
..\..\TivaWareLib.c(35): error: #5: cannot open source input file "utils\ustdlib.c": No such file or directory
3、
..\..\drivers\dac.c(26): error: #5: cannot open source input file "inc/hw_memmap.h": No such file or directory
4、
..\..\drivers\pinout.c(27): error: #5: cannot open source input file "inc/hw_gpio.h": No such file or directory
5、
..\..\drivers\sound_ssi.c(35): error: #5: cannot open source input file "inc/hw_ssi.h": No such file or directory
我都没有发现这些路径和文件,是我少安装了哪些软件吗,我该怎么解决