This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2L: CCS调试连接断开

Part Number: CC2640R2L

CCS启动调试点击运行之后,几十秒后连接断开,报错信息如下:

Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
CS_DAP_0: Power Failure on Target CPU: (Error -180 @ 0x0) The controller has detected a target power loss. The user must turn-on or connect the power supply for the target. (Emulation package 7.0.48.0)
Cortex_M3_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

请问这是什么原因?

  • 您好,

    您用的是什么调试器,XDS还是JTAG?

    CCS版本号是多少?

    硬件问题:如果目标的电源电压未连接到 XDS100v3 的 V Tref信号,通常会出现错误 -180。请仔细检查调试器和目标之间的连接。