This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用CC2540实现一主三从通信(用于无线能量传输)

Other Parts Discussed in Thread: CC2540

我这边有个小项目,希望用CC2540实现一主三从的通信。

用在无线充电的设备里的。大致功能描述如下:

无线充电设备包含两部分,其中的能量发射边为PTU(称为原边),一般为一个无线能量发射板。另一部分为能量接受边PRU(称为副边),一般可以是能量接收的手机壳。在能量发射边,这里选用TI的cc2540作为蓝牙通信设备,以及发射边能量控制设备。(没有其他控制单元)在能量的接收端也选用TI的CC2540作为蓝牙通信设备和输出能量控制设备。

其中原边(能量发射边)的cc2540的作用有,在固定的时间通过IO口使能原边的能量发射装置,从而让置于原边之上的副边得到能量,激发副边的cc2540进行通信,从而确认是否为兼容性的副边设备。如果是兼容的设备,则原边的CC2540一直使能原边的能量发射装置,从而让副边的用电设备即副边的蓝牙设备处于供电状态。副边的cc2540在与原边的cc2540完成连接之后,要通过自身的ADC采样副边的电压和电流,并将之发送给原边的cc2540.原边通过副边发送的电压电流信息判断是否应该持续工作。

有兴趣的朋友可以一起讨论一下。我的QQ390497641.如果有人愿意接这个小活是最好了。

多谢