Using the serial assistant to send the command "0108000304FF0000" can receive a reply "TRF 7970AEVM", and using the upper computer of 7970A can also achieve functions such as reading UID, Blocks, registers, etc. The program burned for TRF7970A is the official "TRF7970A" engineering code, which cannot connect to the upper computer of RF430FRL152H and cannot read the temperature. How can I solve this problem? (Previously, I was able to successfully connect and read the temperature, but after using the JTAG burning program, I was unable to connect to the upper computer.)