This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc430f5137接收状态频频死机

Other Parts Discussed in Thread: CC430F5137, CC1101

问题 描述: 使用cc430f5137一个作为发送端,一个作为接收端。发送端能正常工作,接收端经常死机,一般半小时左右就会死。

                     用的是TI的代码,只要设置ReceiveOn();就会死机,连串口都不通,如果不设置为接收态就没事。 

                   以下为部分代码,请大师解答,谢谢!

void main( void )
{

// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;

Init_IO();
InitButtonLeds();
//WDTCTL = WDT_ARST_250;

SetVCore(0);
delayms(20);

ResetRadioCore();
InitRadio();

ReceiveOn();
receiving = 1;
while (1)

{

}

}
void InitRadio(void)
{
// Set the High-Power Mode Request Enable bit so LPM3 can be entered
// with active radio enabled
PMMCTL0_H = 0xA5;
PMMCTL0_L |= PMMHPMRE_L;
PMMCTL0_H = 0x00;

WriteRfSettings(&rfSettings);

WriteSinglePATable(PATABLE_VAL);
}

void Transmit(unsigned char *buffer, unsigned char length)
{
RF1AIES |= BIT9;
RF1AIFG &= ~BIT9; // Clear pending interrupts
RF1AIE |= BIT9; // Enable TX end-of-packet interrupt

WriteBurstReg(RF_TXFIFOWR, buffer, length);

Strobe( RF_STX ); // Strobe STX
}

void ReceiveOn(void)
{
RF1AIES |= BIT9; // Falling edge of RFIFG9
RF1AIFG &= ~BIT9; // Clear a pending interrupt
RF1AIE |= BIT9; // Enable the interrupt

// Radio is in IDLE following a TX, so strobe SRX to enter Receive Mode
Strobe( RF_SRX );
}

void ReceiveOff(void)
{
RF1AIE &= ~BIT9; // Disable RX interrupts
RF1AIFG &= ~BIT9; // Clear pending IFG

// It is possible that ReceiveOff is called while radio is receiving a packet.
// Therefore, it is necessary to flush the RX FIFO after issuing IDLE strobe
// such that the RXFIFO is empty prior to receiving a packet.
Strobe( RF_SIDLE );
Strobe( RF_SFRX );
}

#pragma vector=CC1101_VECTOR
__interrupt void CC1101_ISR(void)
{
switch(__even_in_range(RF1AIV,32)) // Prioritizing Radio Core Interrupt
{
case 0: break; // No RF core interrupt pending
case 2: break; // RFIFG0
case 4: break; // RFIFG1
case 6: break; // RFIFG2
case 8: break; // RFIFG3
case 10: break; // RFIFG4
case 12: break; // RFIFG5
case 14: break; // RFIFG6
case 16: break; // RFIFG7
case 18: break; // RFIFG8
case 20: // RFIFG9
if(receiving) // RX end of packet
{
// Read the length byte from the FIFO
// RxBufferLength = ReadSingleReg( RXBYTES );
// ReadBurstReg(RF_RXFIFORD, RxBuffer, RxBufferLength);

// Stop here to see contents of RxBuffer
__no_operation();


Flag_rx_over=0x01;
receiving = 0;

}
else if(transmitting) // TX end of packet
{
RF1AIE &= ~BIT9; // Disable TX end-of-packet interrupt
// LEDR_OFF(); // Turn off LED after Transmit
transmitting = 0;

Flag_tx_over=0x01;

}
// else while(1); // trap
break;
case 22: break; // RFIFG10
case 24: break; // RFIFG11
case 26: break; // RFIFG12
case 28: break; // RFIFG13
case 30: break; // RFIFG14
case 32: break; // RFIFG15
}
//__bic_SR_register_on_exit(LPM3_bits);

}