一直没用过TI-RTOS,如何产生EVENT?
用况是这样的,我的定时器每10ms中断一次,我需要在中断中产生一个事件,然后去task中处理。
不同于free-RTOS,在网上找不到任何TI-RTOS这个方面的例程,尽管有文档,全是文字叙述。
有没有可供参考的例程?
此外,2650支持私有协议,但必须基于RTOS,又没有丰富的例程,把简单的事复杂了,而且RF部分的配置实时性还差,虽然是双模的,但在使用的简便性完全不如CC2510,除了处理速度快一点。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
一直没用过TI-RTOS,如何产生EVENT?
用况是这样的,我的定时器每10ms中断一次,我需要在中断中产生一个事件,然后去task中处理。
不同于free-RTOS,在网上找不到任何TI-RTOS这个方面的例程,尽管有文档,全是文字叙述。
有没有可供参考的例程?
此外,2650支持私有协议,但必须基于RTOS,又没有丰富的例程,把简单的事复杂了,而且RF部分的配置实时性还差,虽然是双模的,但在使用的简便性完全不如CC2510,除了处理速度快一点。
首先,你需要创建一个event,例如
/* Create event used internally for state changes */
Event_Params eventParam;
Event_Params_init(&eventParam);
Event_construct(&concentratorEvent, &eventParam);
concentratorEventHandle = Event_handle(&concentratorEvent);
在你的user task中等待event的发生
/* Wait for event */
uint32_t events = Event_pend(concentratorEventHandle, 0, CONCENTRATOR_EVENT_ALL, BIOS_WAIT_FOREVER);
然后,在你的中断处理或者callback函数中post对应event,例如
static void packetReceivedCallback(union ConcentratorPacket* packet, int8_t rssi)
{
/* If we recived an ADC sensor packet, for backward compatibility */
if (packet->header.packetType == RADIO_PACKET_TYPE_ADC_SENSOR_PACKET)
{
/* Save the values */
latestActiveAdcSensorNode.address = packet->header.sourceAddress;
latestActiveAdcSensorNode.latestAdcValue = packet->adcSensorPacket.adcValue;
latestActiveAdcSensorNode.button = 0; //no button value in ADC packet
latestActiveAdcSensorNode.latestRssi = rssi;
Event_post(concentratorEventHandle, CONCENTRATOR_EVENT_NEW_ADC_SENSOR_VALUE);
}
/* If we recived an DualMode ADC sensor packet*/
else if(packet->header.packetType == RADIO_PACKET_TYPE_DM_SENSOR_PACKET)
{
/* Save the values */
latestActiveAdcSensorNode.address = packet->header.sourceAddress;
latestActiveAdcSensorNode.latestAdcValue = packet->dmSensorPacket.adcValue;
latestActiveAdcSensorNode.button = packet->dmSensorPacket.button;
latestActiveAdcSensorNode.latestRssi = rssi;
Event_post(concentratorEventHandle, CONCENTRATOR_EVENT_NEW_ADC_SENSOR_VALUE);
}
}
以上代码示例都来自simplelink_cc13x0_sdk_1_00_00_13中的easylink\rfWsnConcentrator示例
你可以在下面连接找到
http://www.ti.com/tool/SIMPLELINK-CC13X0-SDK