TI的技术支持,您好,在使用CC1101时遇到入下问题,希望帮忙解决
我司使用cc1101是为了学习其他射频遥控器的编码,现在测试使用的频率是433.92MHZ
现在想实现在fsk调制方式下,学习其他公司fsk的遥控器,为了学习fsk调制方式下的遥控器,将cc1101配置为异步直通模式,收集异步直通模式下的电平即可。
测试时使用2块cc1101进行测试,第1个cc1101使用fifo模式发送数据,第2个cc1101使用异步直通模式,收集电平。现在遇到如下问题:
1、在相同速率1.2kbps,相同偏移(Deviation)380khz,,接收滤波带宽为812.5khz情况下,使用示波器能够清晰的看到射频编码信息(高低电平,带有前导码)
在速率配置到100kbps,相同偏移(Deviation)19khz,接收滤波带宽为812.5khz或者改到更小100khz,使用示波器看到的射频编码电平是乱的,即使没有发射机的情况下也会输出电平数据,在有发射机的情况下,也不能清晰的看到射频编码信息
2、cc1101能不能进行扫频,扫描其他遥控器发射的频率,通过检测载波的方式?
3、信号带宽是怎么算的?
4、为什么速率越快,信号带宽会变得越宽
5、速率、信号带宽、频率偏移之间有什么关系?改变速率应该怎么样设置相应的频率偏移?