按照数据手册的参数设置的,0.6Kbaud,GFSK,Dev 14.3K, 58kHz digital channel filter bandwidth,都是按照数据手册设置的,也能通信,就是丢包率达不到数据手册上的1%标准,难道是因为0.6K传输速率太低了吗,数据手册上的0.6KBaud,1%误报率是在严格实验室条件下才能达到吗?求解惑,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我说的频偏是frequency accuracy, 不是Frequency deviation.
你测下来是多少呢?
RXB 就是那个接收带宽。
BR.AZ
CC1101例程参考下面两个链接:
1. http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=swrc021&fileType=zip
这个是基于SmartRF04EB板子写的,开发环境:Keil, 51单片机做主控
2. http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=swrc219&fileType=zip
软件使用手册http://www.ti.com/lit/ug/swru296b/swru296b.pdf
该例程基于 SmartRF TrxEB 开发板,开发环境:IAR, MSP430做主控
另外,关于RSSI, 是一样,但是RSSI寄存器里并不是接收信号强度的绝对值,还需要公式转换,不能直接比较,说明如下:
The RSSI value read from the RSSI status register is a 2’s complement number. The following procedure can be used to convert the RSSI reading to an absolute power level (RSSI_dBm)
1) Read the RSSI status register
2) Convert the reading from a hexadecimal number to a decimal number (RSSI_dec)
3) If RSSI_dec ≥ 128 then RSSI_dBm = (RSSI_dec - 256)/2 – RSSI_offset Note: It takes some time from the radio enters RX mode until a valid RSSI value is present in the RSSI register. Please see DN505 [12] for details on how the RSSI response time can be estimated. CC1101 SWRS061I Page 45 of 98
4) Else if RSSI_dec < 128 then RSSI_dBm = (RSSI_dec)/2 – RSSI_offset