Other Parts Discussed in Thread: CC3200, CC3100
我起振电容尝试过10pf以及15pf,目前用示波器看都没有对应的波形 起振电容的电压 分别为0.6V 和0.8V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据手册,The 32.768K XTAL should be placed closer to the QFN package. Ensure the load capacitance is tuned based on board parasitic so that the frequency tolerance is within ± 150 ppm.
另外,我们有40M晶振的频率调优文档可供参考: http://processors.wiki.ti.com/index.php/CC3100_%26_CC3200_Frequency_Tuning