This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310 rfWakeOnRadio 待机功耗大

Other Parts Discussed in Thread: CC1310, SIMPLICITI

最近在测试CC1310的rfWakeOnRadio例程时,修改唤醒时间间隙为5s,

/* Set next wakeup time in the future */
RF_cmdPropRxSniff.startTime += WOR_WAKE_UP_INTERVAL_RAT_TICKS(WOR_WAKEUPS_PER_SECOND)*5;

发现在这5s期间电流一直是1.14mA,外部晶振测试,是有波形的。而切换到内部时钟,


#ifndef SET_CCFG_MODE_CONF_SCLK_LF_OPTION
// #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x0 // LF clock derived from High Frequency XOSC
// #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x1 // External LF clock
//#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC
#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x3 // LF RCOSC
#endif

CC1310的睡眠电流是1.1uA。

所以请问下外部32kHz的晶振是哪里会影响到功耗呢?谢谢!