使用CC8520,加了CC2590,但是传输距离还是只有10m的样子,大概是怎么回事呢;用的蓝牙模块的天线,天线也换过
附件:配置文件
配置文件可以不可以把发射功率再改大点呢,试验发现穿障碍物的能力也很差,有障碍物3,4m就断了,没有障碍物还可以到将近20m
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这一类问题排查其实都是套路化了。但是如果没有任何测试设备的话,排查比较难的。
你有哪些测试仪器呢?
BR.AZ