Other Parts Discussed in Thread: CC8531, CC8530
各位TI的技术大牛,你们好!
使用CCPW软件将CC8530(自己设计的开发板)与CC8531(官网购买的CC85XX DK 板)烧录同一个配置镜像。CC8531板上GIO9引脚输出NetWork Status LED,1s内有个脉冲信号产生,有效电平维持时间为20ms,空闲时间为980ms。但cc8530板上GIO9引脚每隔10ms输出一个脉冲冲激信号。我对这种现象很不理解,希望各位帮忙解释一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC8531 |
CC8530 |
|
| Device Type | Protocol Processor | Protocol Processor |
| Flash (KB) | N/A | N/A |
| RAM size (KB ) | N/A | N/A |
| Min VCC | 2 | 2 |
| Max VCC | 3.6 | 3.6 |
| RX Current (Lowest) (mA ) | See data sheet | See data sheet |
| Data Rate (Max ) (kbps ) | 5000 | 5000 |
| Modulation Techniques |
8FSK
2FSK
|
8FSK
2FSK
|
| Sensitivity (Best) (dBm ) | -86 | -86 |
| TX Power (Max ) (dBm ) | 3.5 | 3.5 |
| USB 2.0 | Yes | No |
| Features |
Built In audio Protocol
Adaptive Frequency Hoping
High Quality Audio Compression
|
Built In audio Protocol
Adaptive Frequency Hoping
High Quality Audio Compression
|
两者的主要区别在USB。
关于您的问题,请问您是否有使用PurePath 无线配置器 (PPWC) ?根据其说明网络状态 LED为闪烁模式,若是烧录相同程序的话,建议您先检查下您板子的硬件问题而后对程序进行断点调试