Other Parts Discussed in Thread: TMP102, CC1310
下面红色区是里面我比较不懂得地方,不知道为啥要这么写,有人可以指导一下吗
1.为啥rxBuffer[0] 要左移6,rxBuffer[1]要右移2,而且rxBuffer[0] 和rxBuffer[1]是代表啥
2. 不清楚这一段代表意思
3.为啥需要除32,数据有经过什么处理吗
for (i = 0; i < 20; i++) {
if (I2C_transfer(i2c, &i2cTransaction)) {
/* Extract degrees C from the received data; see TMP102 datasheet */
temperature = (rxBuffer[0] << 6) | (rxBuffer[1] >> 2);
/*
* If the MSB is set '1', then we have a 2's complement
* negative value which needs to be sign extended
*/
if (rxBuffer[0] & 0x80) {
temperature |= 0xF000;
}
/*
* For simplicity, divide the temperature value by 32 to get rid of
* the decimal precision; see TI's TMP007 datasheet
*/
temperature /= 32;