This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: CC1352P-4在433MHz基频时,是否支持20dB的PA发射功率?

Part Number: CC1352P

在CC1352P模块中,硬件外围电路设计为433MHz基频时,是否支持20dB的PA发射功率,最大的发射功率是不是13dB,帮忙确认下,谢谢!

  • 在CC1352P模块中,硬件外围电路设计为433MHz基频时,是否支持20dB的PA发射功率,最大的发射功率是不是13dB

    根据 SRRC法规,433M不允许有20dB的发射频率,我记得规定433M最大发射功率应该是10dB,你可以再查一下

    例程中可以设置的最大功率为13dB