This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: cc1200使用情况如下,如何最优设置寄存器?

Expert 2137 points
Part Number: CC1200


尊敬的工程师您好:

 这个问题对我们非常的重要,望您能详细帮我解答下!!! 万分感谢!!!

使用情况如下:

(1)symbol rate = 230.4ksps(由于使用fec,则bit rate =115.2kbps)

(2)工作频率是920mhz左右

(3)工作的晶振是外部温补晶振 40mhz

(4)调制模式2GFSK

(5)使用的是数据包发送模式

(6)此设备是移动的 100m/s

以上这样的情况  deviation、RX Filter BW 、 AGC_REF、 AGC_CS_THR、AGC_GAIN_ADJUST、AGC_CFG3、AGC_CFG2、AGC_CFG1、AGC_CFG0 该如何设置?