433M下,选择输出功率12dbm,软件可以正常编译,正常收发数据;选择13.7dbm,而且修改了,软件编译正常,仿真时提示无法进入DAP错误,能发送几组数据,以后不能正常。请问还有什么需要更改的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SDK版本为。
错误提示为:Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.3.0.00058)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.3.0.00058)
这个错误在选择发射功率大于13时,就会出现;小于等于12时,不出现。如上一个帖子所示,已经修改vddr_hh 为1,但是错误仍在。如果是硬件问题,应该不是复位等问题吧,433M电路参数也是按照手册给的。这个问题一直困扰,项目不能推进。
帮忙看一下吧