This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1125

Other Parts Discussed in Thread: CC1125

1,请问CC1125的频率切换时间有多少?

2,CC1125的邻道抑制在64kbps速率时能做到60dBc吗?它的PDF资料里说是只有47dBc,用的是100kbps滤波器

,假若我用72k滤波器,邻道抑制是不是好些?  434MHz时

  • 临道抑制(ACR),跟调制方式,测量的是100khz间隔。20khz的deviation和100Khz的接收滤波带宽。

    你用72Khz应该会好一些。减小deviation也有助于提高ACR。另外手册给的是db,不是dbc,如果是dbc那还得在47上加芯片本身的发射那就很大了。

    38.4 kbps 2GFSK, 100 kHz channel
    separation, 20 kHz deviation, 100 kHz
    channel filter

  • The lock time of the PLL when
    changing frequencies is 100us-200us (depending on the loop filter), while the time required to
    reprogram the needed registers using a 1 MHz clock is on the order of 50-60us.

  • 1,deviation我理解是频率偏差20kHz,是偏离接收主频吗?不是很明白啥意思,求解惑,谢谢!

    2,acs是指接收的邻道抑制,似乎与芯片本身的发射无关。不是很明白你的说法,求解惑,谢谢!

    3,1125里面有个FEC纠错,它会使速率增加一倍,造成接收灵敏度下降,但也应该会使接收增益增加吧,其纠错能力和解码增益是多大?谢谢!

  • 1,我看1125的收发切换时间才50uS呀!频率切换时我并不需要频率校准。另外有办法来缩短这个频率切换时间吗?最好到40uS.谢谢!

    2,收发切换外部电路怎么设计?是按照参考图上的只改变寄存器设置就行?还是要一个IO口来控制?