This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2540的GATT的一些问题

大家好,我在SimpleBLEPeripheral的工程中添加了一个新的UUID,CHAR6,想在和主机连接之后,接收主机发送的消息,但是现在的问题是,我的主机无法寻找到CHAR6,只是和UUID1而不是UUID6.应该怎么办?

  • lele,

    原因有很多种, 你能描述一下你是怎么定义你的CHAR6 的吗?

    这个CHAR6 的读写属性怎么定义的?

  • 你好Yan,

    我的CHAR6的定义基本是模仿CHAR5来的,属性可读写的,我现在困惑应该是在这里,

    if ( simpleBLESvcStartHdl != 0 )       {         // Discover characteristic         simpleBLEDiscState = BLE_DISC_STATE_CHAR;                 req.startHandle = simpleBLESvcStartHdl;         req.endHandle = simpleBLESvcEndHdl;         req.type.len = ATT_BT_UUID_SIZE;         req.type.uuid[0] = LO_UINT16(SIMPLEPROFILE_CHAR1_UUID);         req.type.uuid[1] = HI_UINT16(SIMPLEPROFILE_CHAR1_UUID);

            GATT_ReadUsingCharUUID( simpleBLEConnHandle, &req, simpleBLETaskId );       },如果我直接把CHAR1改为CHAR6发现还是不能使用,我现在的问题是应该如何让主机搜索到CHAR6...还有就是我可以通过写GATT的哪个函数可以给从机发送ASCII码呢???

     

  • 据我经验看, 

    你这么做是可以的...

    你怎么确定central没有收到呢??  LCD打印?

    发送到peripheral用 write 命令.