This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于RemoTI-CC253xDK-1.3 的配对数量 的修改

Other Parts Discussed in Thread: CC2530

大家好:

           // Network layer implicit constants as in standard used by attribute structure

          #define RCN_MAX_NUM_DEV_TYPES                     3 // number of device types supported per device

         在Remo TI中 如果想要增加配对设备的数量 是否将上面 这个3 修改成需要的值就可以了呢    我试着修改了一下 如我修改成 8  编译后出现了

一下警告:

        Building configuration: rsa_cc2530 - CC2533F96

        Updating build tree...

        rsa_basic.c 

        rsa_osal.c 

        rti.c 

       rti_testmode.c 

      Linking

      Warning[w6]: Type conflict for external/entry "RCN_CbackEvent", in module rcnmac_composite  against external/entry in module rti; function types differ in parameter 1; class/struct/union types  have different sizes

      Warning[w6]: Type conflict for external/entry "RCN_NlmeDiscoveryReq", in module rti against  external/entry in module rcnmac_composite; function types differ in parameter 1; class/struct/union  types have different sizes

     Warning[w6]: Type conflict for external/entry "RCN_NlmeGetPairingEntryReq", in module rti against  external/entry in module rcnmac_composite; function types differ in parameter 2; class/struct/union  types have different sizes

     Warning[w6]: Type conflict for external/entry "RCN_NlmePairReq", in module rti against  external/entry in module rcnmac_composite; function types differ in parameter 1; class/struct/union  types have different sizes  

     Total number of errors: 0

     Total number of warnings: 4

   请问这些警告是怎么回事,

  这个警告我该如何解决? 如果我想要修改配对数量 我该如何修改呢 ,请大家帮助我,给一些建议,谢谢了!