Part Number: LAUNCHXL-CC1350
Other Parts Discussed in Thread: SYSBIOS, CC1350
您好,請問我們正在整合RX和UART,主要是讓兩個裝置能UART用無線相互傳送顯示(uart輸入資料儲存於packet[2],並轉換成INT再TX,RX則是在callback_packet[2]中 ),目前配合smartRF stdio 測試TX應該沒有問題
但RX遇到以下問題:
1.測試傳送"123456789",如果在RX接收成功時執行UART_write第一個字大部分的時候都無法接收(我在RX callbaclk內有printf進行測試)。
2.目前使用RX endtime來關閉RX,因為先使用RX但如果需要TX時,無法將目前正在執行的RX關閉,需要等收到RX訊號後才會TX,不知道目前這個timeout關閉RX的方式是否正確或是標準
程式基本上都是參照RfpacketRX進行修改的,程式碼如下(這是在mainThread內使用task):
/***** Includes *****/
/* Standard C Libraries */
#include <stdlib.h>
/* TI Drivers */
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/UART.h>
#include <ti/sysbios/knl/Task.h>
/* Driverlib Header files */
#include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)
/* Board Header files */
#include "Board.h"
/* Application Header files */
#include "RFQueue.h"
#include "smartrf_settings/smartrf_settings.h"
/***** Defines *****/
/* Packet RX Configuration */
#define DATA_ENTRY_HEADER_SIZE 8 /* Constant header size of a Generic Data Entry */
#define MAX_LENGTH 30 /* Max length byte the radio will accept */
#define NUM_DATA_ENTRIES 2 /* NOTE: Only two data entries supported at the moment */
#define NUM_APPENDED_BYTES 2 /* The Data Entries data field will contain:
* 1 Header byte (RF_cmdPropRx.rxConf.bIncludeHdr = 0x1)
* Max 30 payload bytes
* 1 status byte (RF_cmdPropRx.rxConf.bAppendStatus = 0x1) */
/***** Prototypes *****/
static void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e);
/***** Variable declarations *****/
static RF_Object rfObject;
static RF_Handle rfHandle;
/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;
/* Buffer which contains all Data Entries for receiving data.
* Pragmas are needed to make sure this buffer is 4 byte aligned (requirement from the RF Core) */
#if defined(__TI_COMPILER_VERSION__)
#pragma DATA_ALIGN (rxDataEntryBuffer, 4);
static uint8_t
rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH,
NUM_APPENDED_BYTES)];
#elif defined(__IAR_SYSTEMS_ICC__)
#pragma data_alignment = 4
static uint8_t
rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH,
NUM_APPENDED_BYTES)];
#elif defined(__GNUC__)
static uint8_t
rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH,
NUM_APPENDED_BYTES)]
__attribute__((aligned(4)));
#else
#error This compiler is not supported.
#endif
/* Receive dataQueue for RF Core to fill in data */
/*RX*/
static dataQueue_t dataQueue;
static rfc_dataEntryGeneral_t* currentDataEntry;
static uint8_t packetLength;
static uint8_t* packetDataPointer;
static uint8_t callback_packet[MAX_LENGTH + NUM_APPENDED_BYTES - 1]; /* The length byte is stored in a separate variable */
#define timeout (uint32_t)(4000000*0.1f)
/*RX*/
/*RX Task*/
static Task_Struct rxTask;
#define RX_TASK_STACK_SIZE 1024
static uint8_t rxTaskStack[RX_TASK_STACK_SIZE];
/*RX Task*/
/*TX*/
#define PAYLOAD_LENGTH 30
static uint8_t packet[PAYLOAD_LENGTH];
static uint16_t seqNumber;
int tx_sending = 0;
static uint8_t send_packet[MAX_LENGTH + NUM_APPENDED_BYTES - 1];
/*TX*/
/*TX Task*/
static Task_Struct txTask;
#define TX_TASK_STACK_SIZE 1024
static uint8_t txTaskStack[TX_TASK_STACK_SIZE];
/*TX Task*/
/*Uart*/
UART_Handle uart;
UART_Params uartParams;
char input,output;
/*Uart*/
/*
* Application LED pin configuration table:
* - All LEDs board LEDs are off.
*/
PIN_Config pinTable[] =
{
Board_PIN_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
Board_PIN_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
PIN_TERMINATE
};
/***** Function definitions *****/
void led_init()
{
puts("led_init start");
ledPinHandle = PIN_open(&ledPinState, pinTable);
PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
usleep(300000);
PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
PIN_setOutputValue(ledPinHandle, Board_PIN_LED2,!PIN_getOutputValue(Board_PIN_LED2));
usleep(300000);
PIN_setOutputValue(ledPinHandle, Board_PIN_LED2,!PIN_getOutputValue(Board_PIN_LED2));
if (ledPinHandle == NULL)
{
while(1);
}
}
void rfhandle_init()
{
puts("rfhandle_init");
RF_Params rfParams;
RF_Params_init(&rfParams);
if( RFQueue_defineQueue(&dataQueue,rxDataEntryBuffer,sizeof(rxDataEntryBuffer),NUM_DATA_ENTRIES,MAX_LENGTH + NUM_APPENDED_BYTES))
{
/* Failed to allocate space for all data entries */
while(1);
}
rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
int i = 0;
while(i<10)
{
PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
usleep(100000);
i++;
}
PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,0);
}
void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e)
{
if (e & RF_EventRxEntryDone)
{
/* Toggle pin to indicate RX */
PIN_setOutputValue(ledPinHandle, Board_PIN_LED2, 1);
/* Get current unhandled data entry */
currentDataEntry = RFQueue_getDataEntry();
/* Handle the packet data, located at ¤tDataEntry->data:
* - Length is the first byte with the current configuration
* - Data starts from the second byte */
packetLength = *(uint8_t*)(¤tDataEntry->data);
packetDataPointer = (uint8_t*)(¤tDataEntry->data + 1);
/* Copy the payload + the status byte to the packet variable */
memcpy(callback_packet, packetDataPointer, (packetLength + 1));
printf("%d",callback_packet[2]);
RFQueue_nextEntry();
}
}
void rx_init()
{
puts("rx_init");
/* Modify CMD_PROP_RX command for application needs */
/* Set the Data Entity queue for received data */
RF_cmdPropRx.pQueue = &dataQueue;
/* Discard ignored packets from Rx queue */
RF_cmdPropRx.rxConf.bAutoFlushIgnored = 1;
/* Discard packets with CRC error from Rx queue */
RF_cmdPropRx.rxConf.bAutoFlushCrcErr = 1;
/* Implement packet length filtering to avoid PROP_ERROR_RXBUF */
RF_cmdPropRx.maxPktLen = MAX_LENGTH;
RF_cmdPropRx.pktConf.bRepeatOk = 0;
RF_cmdPropRx.endTrigger.triggerType = TRIG_REL_START;
RF_cmdPropRx.endTime = timeout;
/* Set the frequency */
RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
while(1)
{
if(tx_sending == 0)
{
/* Enter RX mode and stay forever in RX */
RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropRx,RF_PriorityNormal, &callback,RF_EventRxEntryDone);
switch(terminationReason)
{
case RF_EventLastCmdDone:
// A stand-alone radio operation command or the last radio
// operation command in a chain finished.
//puts("RF_EventLastCmdDone");
break;
default:
// Uncaught error event
puts("error1");
while(1);
}
uint32_t cmdStatus = ((volatile RF_Op*)&RF_cmdPropRx)->status;
switch(cmdStatus)
{
case PROP_DONE_OK:
// Packet received with CRC OK
//puts("PROP_DONE_OK");
PIN_setOutputValue(ledPinHandle, Board_PIN_LED2, 0);
output = callback_packet[2];
UART_write(uart,&output,1);
break;
default:
// Uncaught error event - these could come from the
// pool of states defined in rf_mailbox.h
break;
}
}
}
}
void uart_init()
{
UART_init();
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readReturnMode = UART_RETURN_FULL;
uartParams.readEcho = UART_ECHO_OFF;
uartParams.baudRate = 9600;
uart = UART_open(Board_UART0, &uartParams);
if (uart == NULL)
{
/* UART_open() failed */
while (1);
}
}
void rx_task_init()
{
puts("rx_task_init");
Task_Params rxTaskParams;
// TI-RTOS 用來初始化 Task_Params 的API ,這邊會給部分變數預設值
Task_Params_init(&rxTaskParams);
// 有些變數沒有預設值,必須要自行設定
rxTaskParams.stack = rxTaskStack; // 規劃給任務使用的Stack位址
rxTaskParams.stackSize = RX_TASK_STACK_SIZE;
rxTaskParams.priority = 2; // 任務的優先級,數字越大代表該任務越重要
Task_construct(&rxTask, rx_init, &rxTaskParams, NULL);
}
void task_init()
{
puts("tx_init");
RF_cmdPropTx.pktLen = PAYLOAD_LENGTH;
RF_cmdPropTx.pPkt = packet;
RF_cmdPropTx.startTrigger.triggerType = TRIG_NOW;
while(1)
{
UART_read(uart,&input,1);
tx_sending = 1;
PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,1);
RF_yield(rfHandle);
packet[0] = (uint8_t)(seqNumber >> 8);
packet[1] = (uint8_t)(seqNumber++);
uint8_t i;
for (i = 2; i < MAX_LENGTH; i++)
{
packet[i] = rand();
}
packet[2] = input;
RF_EventMask TXterminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx, RF_PriorityNormal, NULL, 0);
switch(TXterminationReason)
{
case RF_EventLastCmdDone:
//puts("TX RF_EventLastCmdDone");
break;
default:
// Uncaught error event
//puts("TX error1");
while(1);
}
uint32_t TXcmdStatus = ((volatile RF_Op*)&RF_cmdPropTx)->status;
switch(TXcmdStatus)
{
case PROP_DONE_OK:
//puts("TX PROP_DONE_OK");
PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
break;
default:
//puts("TX error2");
while(1);
}
tx_sending = 0;
PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,0);
}
}
void tx_task_init()
{
puts("tx_task_init");
Task_Params txTaskParams;
// TI-RTOS 用來初始化 Task_Params 的API ,這邊會給部分變數預設值
Task_Params_init(&txTaskParams);
// 有些變數沒有預設值,必須要自行設定
txTaskParams.stack = txTaskStack; // 規劃給任務使用的Stack位址
txTaskParams.stackSize = TX_TASK_STACK_SIZE;
txTaskParams.priority = 3; // 任務的優先級,數字越大代表該任務越重要
Task_construct(&txTask, task_init, &txTaskParams, NULL);
}
void *mainThread(void *arg0)
{
while(ledPinHandle == NULL)
{
led_init();
}
while(rfHandle == NULL)
{
rfhandle_init();
}
while(uart == NULL)
{
uart_init();
}
rx_task_init();
tx_task_init();
}