This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

手里有一块MSP-EXP430FR5739,能不能用它开发CC1100/CC2420/CC2520/CC2530/CC2540

Other Parts Discussed in Thread: MSP-EXP430FR5739, CC1100, CC2420, CC2520, CC2530, CC2540

如题,买了一块MSP-EXP430FR5739 FRAM Experimenter Board带CC3000模块。因为接口相同,不知道可不可用来直接开发CC1100/CC2420/CC2520/CC2530/2540?比如开发CC2520,如果可以开发的话,可不可以实现CC2520的全部功能?

  • 可以的,CC2520只是一个无线的收发器,所有的配置信息都在MCU端,只要你的MCU和CC2520的连接正确就可以。

  • 由于5739和CC2520的EM的接口已经固定,不存在连接的问题用来开发CC2520应该可以的!但如果自己做一块与CC2520EM接口相同PCB板子,但只把CC2520的SPI、复位、电源和地接到MCU相对应的功能引脚上。把CC2520的GPIO悬空,这样CC2520能不能工作?

    那其他的如CC1100/CC2420/2530/CC2540把GPIO悬空能不能工作?