This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101 睡眠唤醒

Other Parts Discussed in Thread: CC1101

请教Ti工程师,搞了几天了,一直没有结果。我的CC1101怎么都实现不了这个功能。以下是WOR的代码

void  CC1101_InitWOR(void)
{
 //halSpiWriteReg(CCxxx0_SYNC1, 0x38);
 //halSpiWriteReg(CCxxx0_SYNC0, 0x49);

 CC1101_ExitWOR();//sidle模式 

 halSpiWriteReg(CCxxx0_MCSM0,0x18);//在TX,RX后 自动校准  
 halSpiWriteReg(CCxxx0_MCSM1,0x30);
 halSpiWriteReg(CCxxx0_MCSM2,0x09); //RX_TIME_QUAL = 1, RX_TIME = 4

 halSpiWriteReg(CCxxx0_WOREVT1,0x01);// tEVENT0 = 14.34 ms,
 halSpiWriteReg(CCxxx0_WOREVT0,0xF2);
 halSpiWriteReg(CCxxx0_WORCTRL,0x78);// EVENT1 = 3, WOR_RES = 0
 
 halSpiWriteReg(CCxxx0_IOCFG2,0x06); 
 halSpiStrobe(CCxxx0_SWORRST);//复位到 事件1

 
 CC1101_EnterWOR();//启动WOR

}

这样对不对?有没有这方面的例程给参考一下。感谢!!