This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关CC1101的疑问

Other Parts Discussed in Thread: CC1101

我快被CC1101 的WOR功能搞的疯掉了,按照手册AN047和网上的一些资料配置后,就是不能进行唤醒,

设置睡眠15ms,发送采取2.4K的速率,每次发送30个字节。GDO2用做唤醒指示。就是不能实现。如果采取查询寄存器的方式,GDO2会有指示。

 

现在怀疑这个片子是不是具备这个功能?有没有人做过?能不能提供代码以供参考!感谢!!

  • 请把你的寄存器值贴出来

  • 代码如下:

    void  CC1101_InitWOR(void)
    {
     halSpiStrobe(CCxxx0_SIDLE);

     halSpiWriteReg(CCxxx0_MCSM0,0x18);//在TX,RX后 自动校准  
     halSpiWriteReg(CCxxx0_MCSM1,0x30);
     halSpiWriteReg(CCxxx0_MCSM2,0x09); //RX_TIME_QUAL = 1, RX_TIME =1

     halSpiWriteReg(CCxxx0_WOREVT1,0x01);// tEVENT0 = 14.34 ms,
     halSpiWriteReg(CCxxx0_WOREVT0,0xF2);
     halSpiWriteReg(CCxxx0_WORCTRL,0x38);// EVENT1 = 3, WOR_RES = 0
     
     halSpiWriteReg(CCxxx0_IOCFG2,0x06); 
     halSpiStrobe(CCxxx0_SWORRST);//复位到 事件1 
    halSpiStrobe(CCxxx0_SWOR);  //进入WOR状态
    }

    请帮我看看,GDO2用示波器测量一点变化也没有。发送端数据是2.4k波特率。每次发送30个字节。连续发送5次。

    谢谢!!

  • 其他寄存器设置如下:

    //0x00, //FSCTRL2
        0x06,   // FSCTRL1   Frequency synthesizer control.
        0x00,   // FSCTRL0   Frequency synthesizer control.
        0x10,   // FREQ2     Frequency control word, high byte.
        0xB2,   // FREQ1     Frequency control word, middle byte.
        0x3B,   // FREQ0     Frequency control word, low byte.

        0xF6,   // MDMCFG4   Modem configuration.
        0x83,   // MDMCFG3   Modem configuration.
        0x13,   // MDMCFG2   Modem configuration.
        0x22,   // MDMCFG1   Modem configuration.
        0xF8,   // MDMCFG0   Modem configuration.

        0x04,   // CHANNR    Channel number.
        0x15,   // DEVIATN   Modem deviation setting (when FSK modulation is enabled).
        0x56,   // FREND1    Front end RX configuration.
        0x10,   // FREND0    Front end RX configuration.
        0x18,   // MCSM0     Main Radio Control State Machine configuration.
        0x16,   // FOCCFG    Frequency Offset Compensation Configuration.
        0x6C,   // BSCFG     Bit synchronization Configuration.
        0x03,   // AGCCTRL2  AGC control.
        0x40,   // AGCCTRL1  AGC control.
        0x91,   // AGCCTRL0  AGC control.

        0xE9,   // FSCAL3    Frequency synthesizer calibration.
        0x2A,   // FSCAL2    Frequency synthesizer calibration.
        0x00,   // FSCAL1    Frequency synthesizer calibration.
        0x1F,   // FSCAL0    Frequency synthesizer calibration.
        0x59,   // FSTEST    Frequency synthesizer calibration.

        0x81,   // TEST2     Various test settings.
        0x35,   // TEST1     Various test settings.
        0x09,   // TEST0     Various test settings.
        0x0b,   // IOCFG2    GDO2 output pin configuration.
        0x06,   // IOCFG0D   GDO0 output pin configuration. Refer to SmartRF?Studio User Manual for detailed pseudo register explanation.

        0x67,//0x04,   // PKTCTRL1  Packet automation control.可变数据包长度
        0x05,   // PKTCTRL0  Packet automation control.
        0x49,   // ADDR      Device address.
        0x20,    // PKTLEN    Packet length.

  • http://www.deyisupport.com/question_answer/analog/wireless_connectivity/f/45/p/8173/103717.aspx#103717

    有source code,供参考。