MCU是MSP430F149,一块板子一直发送数据,一块板子接收数据,使用仿真读出RX-FIFO可以确定数据已经可以收到,但是无论如何GDO脚都不置位,这是为什么啊???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是参考的 CC1101 Datasheet Page 62 吗?
Table 41: GDOx Signal Selection (x = 0, 1, or 2)
你好,Nutcracker!我使用CC1101的时候,遇到了接收端GDO0引脚一直为低,没能正常跳变的问题。我是用的MCU是STC12LE5A60S2,一个板子发送数据,另外一块板子接收数据。发送数据的时候,GDO0引脚有正常的跳变。
我的寄存器配置信息如下:
uint8 code radioSettings[] =
{
0x24, // IOCFG2 GDO2 output pin configuration.
0x2E, // IOCFG1 GDO1 output pin configuration
0x24, // IOCFG0 GDO0 output pin configuration
0x07, // FIFOTHR RX FIFO and TX FIFO thresholds
0xD3, // SYNC1 Sync word, high byte
0x91, // SYNC0 Sync word, low byte
0x05, // PKTLEN Packet length
0x04, // PKTCTRL1 Packet automation control
0x04, // PKTCTRL0 Packet automation control
0x00, // ADDR Device address
0x00, // CHANNR Channel number
0x06, // FSCTRL1 Frequency synthesizer control // 0x06->10Kbps; 0x08->250Kbps
0x00, // FSCTRL0 Frequency synthesizer control
0x10, // FREQ2 Frequency control word, high byte
0xA7, // FREQ1 Frequency control word, middle byte
0x62, // FREQ0 Frequency control word, low byte
0x78, // MDMCFG4 Modem configuration
0x93, // MDMCFG3 Modem configuration
0x03, // MDMCFG2 Modem configuration
0x22, // MDMCFG1 Modem configuration
0xF8, // MDMCFG0 Modem configuration
0x44, // DEVIATN Modem deviation setting
0x07, // MCSM2 Main Radio Control State Machine configuration
0x30, // MCSM1 Main Radio Control State Machine configuration
0x18, // MCSM0 Main Radio Control State Machine configuration
0x16, // FOCCFG Frequency Offset Compensation configuration
0x6C, // BSCFG Bit Synchroni zation configuration
0x43, // AGCTRL2 AGC control
0x40, // AGCTRL1 AGC control
0x91, // AGCTRL0 AGC control
0x87, // WOREVT1 High byte Event 0 timeout
0x6B, // WOREVT0 Low byte Event 0 timeout
0xF8, // WORCTRL Wake On Radio control
0x56, // FREND1 Front end RX configuration
0x10, // FREND0 Front end RX configuration
0xE9, // FSCAL3 Frequency synthesizer calibration
0x2A, // FSCAL2 Frequency synthesizer calibration
0x00, // FSCAL1 Frequency synthesizer calibration
0x11, // FSCAL0 Frequency synthesizer calibration
0x41, // RCCTRL1 RC oscillator configuration
0x00, // RCCTRL0 RC oscillator configuration
0x59, // FSTEST Frequency synthesizer calibration control
0x7F, // PTEST Production test
0x3F, // AGCTEST AGC test
0x88, // TEST2 Various test settings
0x31, // TEST1 Various test settings
0x0B, // TEST0 Various test settings
};
IOCFG0的值我设置为0x06,就是在接收时遇到了GDO0一直为低,不能正常跳变的问题。
非常期待您的回答。
Thank U in advance.
Best regards.