This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2500传输距离,灵敏度测试?

老大没买评估板,也不知道正不正常:

250kbps:20m (极限有效距离),随意有效距离:2m

500kbps:13m(极限有效距离),随意有效距离:9m

接收板:收到一包回一包

发射板:每隔0.5s发一包,然后立刻进入接收状态,如果收到则闪灯,如果能看到连续稳定闪灯,则认为是有效距离。

极限有效距离:拿在手上,精确对准

随意有效距离:放地上,无障碍物,不精确对准

Datasheet中的灵敏度是在1%误包率下测试的,测误包率的方法是不是这样:固定发N个数据包,看接收到了多少包?

关于灵敏度测试方法:

1.对于单极天线可以用透明模式测试吧。

2.对于PCB天线有没有好的测试方法?