请教问题:(1)CC1000无线传输芯片可以发射不经调制可变频的正弦信号么?(2)如果要进行正弦信号发射,在TXBUF内应该存储什么值呢?(2)可发射正弦信号的频率范围是多少呢?怎么对其进行变频呢? 非常感谢啦
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这位朋友还在用 CC1000啊?这颗芯片真的是非常古老了。你的意思是输出基带信号?还是单载波信号?
呵呵,因为刚刚接触所以劳烦大神了,想用CC1000发射单载波信号,用于相移测距,(这是我最近看到的一个思路,版主用的CC1000,想试试),但是我手头上用的CC1101,我觉着CC1101不适合的原因可能在于(1)不能像CC1000那样发射可变频的载波,因为CC1101的频率就用寄存器进行的配置,应该不能够自动进行变频,但是CC1000支持跳频协议(2)CC1000支持RSSI/IF信号输出,但我也感觉CC1101虽然没有RSSI输出口,但从寄存器中读取的RSSI值应该也是可以反映其中频信号输出的(虽然不知道对不对,但觉着这第2点CC1101应该也可以实现)。可否请教一下大神CC1000在变频和单载波发射方面怎么进行设置吗?非常感谢啦