This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200 与CC430F5137之间的MSK通信问题

Other Parts Discussed in Thread: CC1200

CC1200 配置2-FSK调制,速率250kbps,调制频偏62.5KHZ,(相当于MSK调制)它发送数据,

CC430配置为MSK调试,速率250kbps,它无法接受到CC1200发送的数据,但将CC430的调制方式改为2-FSK,频偏设为62.5KHZ,是可以收到CC1200发送的数据的。

还有,我用2个CC430,一个设为2-FSK调制,一个设为MSK调制,它们之间是可以通信的,为什么CC430的MSK就是不能和CC1200进行通信呢??

     MSK是2-FSK的一种特殊调试方式,应该说CC430的2-FSK调制都能与CC1200通信,那么MSK调制也能通的,但事实就是不行?有没有知道是怎么回事的大神们,请指点一下。

  • CC1200是一颗窄带的芯片 正确接受需要比较准确的频点

    建议您可以做如下测试 从CC1200发送CC430接收 如果可以则需要细调CC1200的配置 如果不行 还是建议您使用同样的2-FSK的调制方式