This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1312R1: 同时使用2个串口编译报错

Part Number: LAUNCHXL-CC1312R1
Other Parts Discussed in Thread: CC1312R

Hi team,

我看到CC1312R支持2个串口,我也配置了uart1的对应rx/tx的DIO口

在使用时,为了分别对串口进行配置,我想要用2个UART_Handle句柄和UART_Params参数结构体进行后续配置,可是我发现,UART_Handle只能命名为uart,UART_Params只能命名为uartParams,
一旦更名就会报错

#10010 errors encountered during linking; "xxx_CC1312R1_LAUNCHXL_tirtos_ccs.out" not built
#10234  unresolved symbols remain

这是为什么?
如果我想要对两个串口分别进行不同的配置,应该怎么办?
谢谢