This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1100E的同步字检测问题?

请教CC1100E的同步字检测中断的设置问题:

    试验发现,采用以下的中断设置和函数,当TI_CCxxx0_IOCFG2=0x07、即接收到CRC_OK时产生中断,程序能正常地待机和接收到数据;但当TI_CCxxx0_IOCFG2=0x06、即设置为接收到同步字时产生中断,则会不断地进入中断,而此时并没有模块在发送,即很容易地误触发同步字中断。

    请问如果需要采用检测到同步字时才产生中断,应该如何设置(包括各相关的寄存器的设置)?


//====================== GDO2的外部中断设置 ====================
void GDO2_ISR(void)
{
  TI_CC_GDO2_PxSEL &=~TI_CC_GDO2_PIN;      // 普通IO
  TI_CC_GDO2_PxDIR &=~TI_CC_GDO2_PIN;       // input
  TI_CC_GDO2_PxREN |= TI_CC_GDO2_PIN;       //
  TI_CC_GDO2_PxOUT &=~TI_CC_GDO2_PIN;       // Set P2.1 as pull-Down resistance 
  TI_CC_GDO2_PxIES &=~TI_CC_GDO2_PIN;       // P2.1 Lo->Hi edge
  TI_CC_GDO2_PxIFG &=~TI_CC_GDO2_PIN;       // P2.1 IFG cleared
  TI_CC_GDO2_PxIE |= TI_CC_GDO2_PIN;         // P2.1 interrupt enabled,GDO2
}


//*******************以下为中断函数**************************
// P2.1 GDO2中断服务(Lo->Hi上升沿中断)
#pragma vector = PORT2_VECTOR
__interrupt void port2_ISR (void)
{
  if(P2IFG & TI_CC_GDO2_PIN)                    // Command received from RF
  {                                                    // RX active
    P2IFG &= ~TI_CC_GDO2_PIN;                   // Clear Receive flag
    __bic_SR_register_on_exit(LPM3_bits);      // Clear LPM3 bits from 0(SR)
    TACCTL0 &= ~CCIE;                              // Disable timer Interrupt   
    P2IFG &= ~BIT1;                                 // P2.1 IFG cleared
    P2IE &= ~BIT1;                                  // P2.1 interrupt disabled,GDO2
  }
}

 

  TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG2,   0x07);

  TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG0,   0x06);

  • 测试通过的代码,你试试

    #define BIT2                (0x0004u)

    #define GDO2 BIT2 //I //P1IN

    void InitPort1Interrupt(void)

    {

     P1IFG &= ~GDO2;     // Clear flag

     P1IES  |= GDO2;        // Int on falling edge (end of pkt)      

     P1IE     |= GDO2;       // Enable int on end of packet

    }

    #pragma vector=PORT1_VECTOR

    __interrupt void ISR_PORT1 (void)

    {

     if (P1IFG&GDO2)

     {

       P1IFG  &= ~GDO2;

       radioRxFlag = 1;

       LPM3_EXIT;

     }

    }