1. CC2590是一款射频放大器。不过在产品技术文档中有2大问题不是很清楚:射频阻抗匹配以及TXRX的控制。
2. 对于CC2590来言,阻抗匹配包括2个部分,
2.1 输入RF-N和RF-P的阻抗匹配,对于CC2xxx系列来说,输出阻抗匹配都是50欧姆,但是在CC2590.pdf文档中,区别CC24xx,CC2500和CC2511给出了不同的阻抗匹配方式,而在CC2541-CC2590参考设计中却采用了附加的匹配回路。问题是:cc2590对于不同的射频芯片是否匹配回路有区别。这个CC2541-CC2590标准设计,是否可以用在CC2650-CC2590的设计中。
2.2 ANT的天线输出阻抗匹配。当采用板载PCB天线时,阻抗匹配还是50欧姆吗,也就是说,射频收发器芯片经过CC2590射频放大,天线部分是否可以保持不变。
3. 对于CC2590的EN,PAEN,HGM引脚的RXTX控制和增益控制,是需要对TI提供的协议栈进行修改吗。也就是说,如果CC2650程序代码,在增加了CC2590之后是否要进行修改。