Other Parts Discussed in Thread: CC3200SDK, CC3200
CCS中编译oslib时出现如下信息:
**** Clean-only build of configuration free_rtos for project oslib ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k clean
DEL /F "free_rtos.a"
DEL /F "croutine.d" "heap_3.d" "list.d" "osi_freertos.d" "port.d" "queue.d" "tasks.d" "timers.d"
DEL /F "croutine.obj" "heap_3.obj" "list.obj" "osi_freertos.obj" "port.obj" "portasm.obj" "queue.obj" "tasks.obj" "timers.obj"
DEL /F "portasm.d"
找不到 C:\ti\CC3200SDK_1.2.0\cc3200-sdk\oslib\ccs\free_rtos\free_rtos.a
找不到 C:\ti\CC3200SDK_1.2.0\cc3200-sdk\oslib\ccs\free_rtos\croutine.d
找不到 C:\ti\CC3200SDK_1.2.0\cc3200-sdk\oslib\ccs\free_rtos\croutine.obj
找不到 C:\ti\CC3200SDK_1.2.0\cc3200-sdk\oslib\ccs\free_rtos\portasm.d
'Finished clean'
' '
**** Build Finished ****
Buildfile generation error occurred..
This project was created using a version of compiler that is not currently installed: 5.2.6 [ARM]. Please go to CCS App Center to install the compiler of this version, or migrate the project to one of the available compiler versions by adjusting project properties.
Build stopped..
错误描述如下:
Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 5.2.6 [ARM]. Please go to CCS App Center to install the compiler of this version, or migrate the project to one of the available compiler versions by adjusting project properties. oslib properties Problems
根据Programmer's Guide,Oslib • Contains the interface file to configure Free-RTOS or TI-RTOS.我下载了TI-RTOS CC32xx。
新手上路,请大神不吝赐教。