你好 ,想问一下CC3200中我用flash存储数据,是不是关闭WiFi后也会把文件系统中的一些东西给关掉,请问如何解决呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果关闭的WiFi,也就将SPI Flash的写入等操作关闭了,因为文件数据的写入 SPI Flash是通过内部总线的WiFi 处理器NWP内核完成的。
同时更新一下WiFi CC3200的升级芯片CC3220的基本信息:
The CC3220 family offers three pin-to-pin compatible variations:
CC3220SF芯片内置了 1MB的Flash,客户的代码直接在Flash中运行,256k的RAM完全开放给客户使用,同时增加了Security的支持
CC3220S芯片使用256k的RAM同时运行代码和RAM,也就是代码+程序使用的RAM在256k范围之内,增加了Security的支持
CC3220R芯片内置256k的RAM,
最新的CC3220升级芯片在AP模式下可以支持最大4个Station的连接,同时增加了IPV6的支持,增强了wifi RF的设计,大幅度提升了SmartConfig的配置成功率,详细了新特性的增加请参考CC3220的芯片手册和设计指南。