This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

simplink 适用手机

Other Parts Discussed in Thread: CC3200, CC3220SF, CC3220S, CC3220R

测试过比较多的手机进行simplink联网绑定路由器,在苹果手机上6s以上有可以用的么

  • 通过手机配置CC3200、CC3220连接到指定的路由器上的功能称作为SmartConfig, 这个功能在苹果6S上可以使用的,而且绝大多数的智能手机都可以使用该功能

     CC3200的升级芯片CC3220的基本信息:

    The CC3220 family offers three pin-to-pin compatible variations:

    • CC3220SF: 256kB RAM + 1MB XIP Flash and application level security
    • CC3220S:   256kB RAM and application level security
    • CC3220R:   256kB RAM

    CC3220SF芯片内置了 1MB的Flash,客户的代码直接在Flash中运行,256k的RAM完全开放给客户使用,同时增加了Security的支持

    CC3220S芯片使用256k的RAM同时运行代码和RAM,也就是代码+程序使用的RAM在256k范围之内,增加了Security的支持

    CC3220R芯片内置256k的RAM,

    最新的CC3220升级芯片在AP模式下可以支持最大4个Station的连接,同时增加了IPV6的支持,增强了wifi RF的设计,大幅度提升了SmartConfig的配置成功率,详细了新特性的增加请参考CC3220的芯片手册和设计指南。